This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how i can use analog camera with OMAP4430

hi,

I want to use analog camera with OMAP4430. Output from analog camera will be either NTSC or PAL serially. I am little bit confused what should i use and what should be the sequence? like should i use sequence

1-  Camera - video decoder & ADC (to convert signal in to BT-656 standar) - BT656 to CSI-2 converter

2-  camera - ADC - BT656 to CSI-2 converter

or is there any other sequence should i follow?

one another question does OMAP4430 have internal video decoder and encoder? and does it can detect wether camera is giving input in NTSC or PAL?

 

regards,

Ankush agrawal