This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NDK DaeMon within a Task



Hi Ti Folks,

                 I am stuck in understanding this NDK TCP/IP Daemon within a Task.

I have created a task using Task_create with a stack size of 4096 bytes 

and within that task i am using this function

extern HANDLE DaemonNew( uint Type, IPN LocalAddress, uint LocalPort,int (*pCb)(SOCKET,UINT32), uint Priority,uint StackSize, UINT32 Argument, uint MaxSpawn );

and i am using following values [Task Priority as Normal and Stack size as normal] and they correspond to below values

#define OS_TASKPRINORM_DEF      5

#define OS_TASKSTKNORM_DEF      4096

If you look at above lines, i am creating a task with stack size of 4096 bytes within which i am creating a NDK daemon which is taking exactly 4096 bytes as stack size.

my questions on above.

1. where does the ndk daemon get the stack allocated from? [is it from global source or from the Task itself..please clarify]

Thanks

RC Reddy