Other Parts Discussed in Thread: TMS320C6657
Hi all,
As mentioned in sprugy5b there is a DDR configuration table that can be used to set up external memory during a boot. My questions are whether this functionality is available during the Ethernet Boot mode for the TMS320C6657 (the main goal is to configure the DDR and load the program into DDR without using any secondary boot loaders), and if it is, where in the L2 memory is the table located during the boot process?
I also noticed that the c6657 technical data sheet (sprs814a) mentions that the starting address for the section of the L2 SRAM that the boot loader uses is 0x00872DC0, is this correct or should it be 0x008F2DC0?
Thanks,
Mark