Other Parts Discussed in Thread: PCM3168A, TAS5086, TAS5631B, CC2560
I'm wondering if the OMAP-L13x is suitable for interfacing a PCM codec(PCM3168A), an audio PWM processor (TAS5086) and Power Amp (TAS5631B). In another application I want to use the same processor but it needs to interface with the PCM codec and a Bluetooth Controller (CC2560). The end products are for an Audio Controller and PA system.
This processor seems a little overkill but needs to handle interrupts and audio signal processing. There are just too many options out there and they all seem to be tailored to Video or more complex situations than I require.
Any help would be greatly appreciated.