This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3 EVM Rev D (processor revB) - Reflash X-Loader and U-boot with flash 1.6 tool



Hi !

I did wanted to test dvsdk v4.01 on the EVM platform.

Infortunately I flash u-boot and it does not start on platform reset.

I tried to reflash it through flash utility v1.6.

Things get worst when by mustake I erase X-Loader.

Here are the steps I followed :

Fisrt I modified omapflash2nd.txt for nand recognition : CUSTOM_OMAP35XX_BOARD 343007 57 => CUSTOM_OMAP35XX_BOARD 343007 54

Then I modified configuration_evm35xx_micron_512m.txt because its nand address was 0x28000000, and conforming to hardware user guide the nand was at 0x20000000.

I recomplied X-Loader and signed it to get the ift file.

Now I launch the flash utility with config=OMAP35x, ECC Style=HWECC, file = x-load.bin.ift.

At startup the XLoader does not boot .

Worst If I relaunch the flash tool just to erase the x-loader region I get stuck in the middle of the process :

¯ -stdout

¯ -omap 3

¯ -no_force_package_alignment

¯ -com 1

¯ -t 60

¯ -p EVM_MDDR_MICRON_512M

¯ -2

¯ chip_erase NANDINFO1BITBOOT 00080000

¯ Leaving parameter file:temp_script.txt

¯ @temp_script.txt

¯ Looking for device (omap com1)

¯ Please turn off device, then turn it on again

¯ Awaiting ASIC id

¯ Awaiting ASIC id

¯ AsicId items 04

¯ AsicId id 01 05 01 34 30 07 54

What can I do know ?

Are my parameters correct ?