This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

YUYV input format in 8bit mode

Hi,

We are using the DM8148 EVM to capture video from a custom source. We are using HDVPSS VIN0A in 8bit single channel mode with discrete sync. We are able to make the capture but the chroma / luma ordering is wrong because the HDVPSS expects the input format to be UYVY but our video source can only support YUYV. Is there a way we can modify the HDVPSS source to support the order switching of chroma / luma? Or is there any hardware in HDVPSS that can do the switching? We are using DVR-RDK 3.0.0

Thanks in advance,

Tim