Other Parts Discussed in Thread: ADS1274
Dear TI
I'm working with a DSK6455 kit and an ADS1274 acquisition board. I use CCS v4.2.5.005. I need to send a data buffer from the dsk to a PC server. I use the NDK kit:
client.c for the configuration ethernet.
main.c to configure mcbsp, spi, interrupts an other parts of the ADS1274.
sender_tcp.c to management the data sending. It's based in your sender.c example, but I use TCP protocol.
The dsk and the PC are connected to a switch, only them. In this conditions the system works perfectly.
The problem appears when I connect the switch to a plug on the wall where there are public addresses. At that moment the data sending fails and locks the system.
I've tested the system and the problem is in the function "connect". It returns -1 and with fdError() I can see that the error is number 55 (ENOBUFS 55 // No buffer space available). Well, but, what buffer?
I've tested the wire with wireshark and I can see a lot of ARP protocols, can they be responsible of the problem?
Could you help me, please?
Best regards.
Manuel Fernández Ros