Hi Experts,
There are two SGMII ports in C6678, my ctms want to specify the port for transmission. To specify the transmit port for the packet, I think it is need to configure the ALE switch, but I cannot find the NDK API to configure the ALE switch. After going through the MCSDK and PDK NDK examples, I think it is need to call the LLD API such as init_cpsw, right? Would u pls kindly instruct how to achieve it and which API can be used if possible?
Thanks & Best Regards,
Andy