This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hunting for a library



I am working with the ex08_ringio code, specifically the dsp side of this code.  To begin, I am trying to insert this snippet of code from the Eric & Scott Sys/Bios Workshop:

//-----------------------------------------------------------------------------
// USTIMER_delay()
//
// LogicPD BSL fxn - re-written for a few BSL.c files that need it.
// The original USTIMER_init() is not used because it is NOT BIOS compatible
// and took both timers so that BIOS PRDs would not work. This is a
// workaround.
//
// If you need a "delay" in this app, call this routine with the number
// of usec's of delay you need. It is approximate - not exact.
// value for time<300 is perfect for 1us. We padded it some.
//-----------------------------------------------------------------------------

void USTIMER_delay(uint32_t usec) {
    volatile int32_t i, start, time, current;

    for (i=0; i<usec; i++) {
        start = Timestamp_get32();

        time = 0;

        while (time < 350) {
            current = Timestamp_get32();
            time = current - start;
        }
    }
}

I have also added:

#include <xdc/runtime/Timestamp.h>

Now at link time I am receiving:

 undefined                      first referenced            
  symbol                            in file                 
 ---------                      ----------------            
 xdc_runtime_Timestamp_get32__E bin/debug/obj/main_dsp.oe674

error: unresolved symbols remain

I cannot seem to locate which library to include in my build at this point.  Which library do I need?  A grep shows multiple libraries which contain this symbol.

  • The likely cause of this is that your configuration file (*.cfg) doesn't include a reference to the module you are trying to use in the application.

    You can add the following to your *.cfg file.

    var TimeStamp = xdc.useModule('xdc.runtime.Timestamp');