This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM 8148 Capture VIN 0 YUV data by using Appro Camera Release 3

Expert 1840 points

Dear Sir / Madam,

I am working with a custom board using DM8148 ti CHip. We used the HD-SDI (YUV 16 bit) as video input into VIP0.

My question is: We want to use the software Rel 3 of Appro camera DM 8148 but replace camera interface by Capture interface. Is it possible or not?

I have already looked through the source code and usecase of these mcfw of release 3.0 and I think it may be ok, I am not sure 100% so I ask for a confirm.

If it is ok, so can you give a suggestion for quick modification? 

I am really thanks for your supports.