Hi we are using the C6748 DSP and I have a question on fan out of the AHCLKX and AHCLKR pins.
Our external crystal is 22.5792 Mhz running 451.584 Mhz internally.
I have one SPI device on the McASP and 2 SPI devices on McBSP. I want to feed 3 external SPI devices SYSCLK's with the 22.5792 Mhz and was hoping I could use the AHCLKX output of the McASP. My question is can this pin drive the 3 devices? Also is there a better way to do this?
Thanks, John