Other Parts Discussed in Thread: TMS320C6748
Hello all,
I am now using TMS320C6748 device on our system.
Our current phase is to select power supply device for this system.
Then, I am referring your application note, High-Efficiency Power Solution Using DC/DC Converter With DVFS; SLVA341A.
On page2, I could find out Imax value for this device, which describes that;
RTC_CVDD Imax = 1mA Static 1.2V Imax = 200mA
I think the total Imax value for 1.2V line is 201mA.
Meanwhile, I could find out another table on page3, which describes Static 1.2 V + VRTC at 251 mA.
Could you let me clarify which Imax (201mA or 251mA) is correct?
Also, regarding 3.3V line, I found different point for Imax value.
Page2: Static 3.3V Imax = 24mA DVDD3318 3.3V Imax = 90mA
Page3: Static 3.3 V at 115mA
Could you let me clarify which Imax (114mA or 115mA) is correct?
Thank you in advance for your information.
Best regards,