This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Encode example application in ezsdk5.04 with DM8168



Hi,

I have installed ezsdk 5_04_00_11. I have build omx and its example applications successfully.

I am trying to running encode example application with bellow mention parameters,

./encode_a8host_debug.xv5T -i sample.yuv -o sample.h264 -f 60 -b 1000000 -w 1920 -h 1080 -c h264

here I am giving 1920*1080 yuv420semiplanner with 60 fps 1000000 bitrate as a input which gives me encoded (h264) output in sample.h264.

But When I play sample.h264 in my VLC player, the quality of the video is not appropriate and seems different from the input.

Am I doing anything wrong with this ?

Note: I am using DM8168 multimedia processor.

Quick response will be appreciated.

Shabbir Limdiwala