I had a problem with connecting ccs5.1.0 to FDK kit. I'm getting the following error code when clicking on connect target button,
"C55xx: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the emulator can be located. (Emulation package 5.0.663.0) "
My Hardware Spec:
> IDE CCS5.1.0
> C5515 FDK ,optical sensor
> Windows platform.
Problem's facing:
1. It can't switch the mode from normal to User Bios mode.
2. When i connect devices with mini USB alone, system doesn't response. I mean in device manager window nothing is displaying.
3. Only the Type B detected and driver has installed automatically. In the device manager window shows TI Channel A, TI channel B.
Queries:
1. Should i have to install any drivers like FTDI.
2. I can't get the driver for FT2232D0708 chip. Where i can download it?
3. The mode can be change automatically or we have to press the DIP switch.