This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About Gen2 operation with x2 link on PCIe of DM8168

Guru 10570 points

Hello.

I would like to use DM8168 as PCIe root.
I need spec gen2 and x2 link.

Can I confirm if there are some restriction or errata?

Best regards,
RY

  • Hi RY,

    According to the DM816x Datasheet, your use case is available:

    PCIe® port x2 lanes GEN2 compliant interface, which allows the device to act as a PCIe® root complex or device endpoint;

    The device PCIe supports the following features:
     - Supports Gen1 and Gen2 in x1 or x2 mode

    There is one bug described in the Silicon Errata which seems related:

    Advisory 2.0.44  PCIe Gen2 Mode: PCIESS Corruption of Round-Trip Latency Time and Replay Time Limit Bits (PL_ACKTIMER Register)

    Revisions Affected: 2.0, 1.1, 1.0

    Details: When the PCIe is operating in Gen2 mode (5-Gbps rate per PCIe link in each direction), writing to either of these bits, round trip latency time limit (RND_TRP_LMT) or the replay time limit (RPLY_LIMT), in the PL_ACKTIMER register causes the value of the bit field that was not being updated to also be modified, corrupting the register contents.

    Workaround: Ensure that any updates to either the RND_TRP_LMT or the RPLY_LIMT bits in the PL_ACKTIMER register are made only when the PCIe is operating in Gen1 mode (2.5-Gbps rate per PCIe link in each direction).

    Regards,

    Pavel




  • Hello, Pavel.

    Thank you so much for your support.
    I will check this !

    Best regards,
    RY