Other Parts Discussed in Thread: AM3352
Hi Mr,
The reference manual of AM3352 show that it support for large page size (2048 bytes + 64 spare bytes) or very large page size 4096 bytes + 128 /
218 spare bytes) when booting from NAND flash. We select a 8Gb 16 bit Micron Flash (MT29F8G16ABACAWP:C), it page size is as below:
– Page size x8: 4320 bytes (4096 + 224 bytes)
– Page size x16: 2160 words (2048 + 112 words)
Can this flash be supported by AM3352?
And the reference manual of AM3352 show that it "only supports devices where Chip Select can be de-asserted during read, program or erase cycles,
without interrupting the operation". Does this feature exist on normal NADN flash, such as Micorn/MT29F8G16ABACAWP:C?
Thanks a lot!
Best Regards,
Cosmo