This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x Linux application queries



Hi Champs,

One of my customers is using an AM335x board. There are some issues:

1) ADC Access

Not able to access ADC port tsc as  it is listed in /proc file system. The iomem command shows the names of all I/O mapped devices with their physical addresses. The programmer should be able to access those devices with names in their drivers/code. As of now very few devices  like UART3 timer are accessible

Any idea/sample app you can share to use ADC ?

2) UART app issue

Also he could wirite on UART3 with /dev/ttyO3 but could not see the output on Hyperterminal or minicom. The simple code is attached in the mail.

Any prompt inputs will be great to have

Best Regards

Feroz