Hello,
I use the uPP of the TMS320C6655 connected to an FPGA and I also have a NAND flash connected to EMIF16 to store data.
How can I use both? The interfaces share the pins. Is it both distinguished by writing to different memory addresses, because both peripherals are mapped on different addresses in the memory map? For this case I also connected the /CS signal which is used by the NAND flash to the FPGA, to enable the FPGA to recognize whether the NAND flash is addressed or not. Can this work?
Thanks for your help.
Best regards,
Michael.