Other Parts Discussed in Thread: TPS65070
When setting operational point to 456MHz UBL reprograms TPS65070 to change VDCDC3 from 1.2V to 1.3 V.
The DEFSLEW register is not modified by UBL when operational point changes (default value 7.2 mV/us).
OMAP L-138 datasheet specifies that "The maximum voltage slew rate for CVdd supply changes is 1 mV/us."
Is fast slew rate going to cause us problems?