This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6657 emac_open in forever loop

Hi,

  WHen I run the client example for the 6657 I receive these messages in the console:

C66xx_0]

[C66xx_0] TCP/IP Stack Example Client

[C66xx_0] emac_init: core 0, port 0, total number of channels/MAC addresses: 1/1

[C66xx_0] MAC addresses configured for channel 0:

[C66xx_0] 08-00-28-32-96-AC

[C66xx_0] SGMII reset successful........

[C66xx_0] SGMII config successful........

 

when I halt the processor I am always in the emac_open function and never exit. 

Thanks,

Will