Other Parts Discussed in Thread: AM3359
i have BeagleBone Board(AM3359), (Add SPI FLash (W25Q64CV))
I tries to operate as spi multi-channel mode (SPI0->CS0,CS1)
this code is setting sequence..
///////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
#define MCSPI_IN_CLK 48000000
#define MCSPI_OUT_CLK 24000000
#define SPI_CHAN 0x0
#define SPI_CHAN1 0x1
#define SPI_BASE SOC_SPI_0_REGS
#define SPI_BASE1 SOC_SPI_1_REGS
void SPI_Initialize(void)
{
unsigned int retVal = 0;
unsigned int regVal;
/* Enable clock for SPI */
regVal = (HWREG(SOC_CM_PER_REGS + CM_PER_SPI0_CLKCTRL) &
~(CM_PER_SPI0_CLKCTRL_MODULEMODE));
regVal |= CM_PER_SPI0_CLKCTRL_MODULEMODE_ENABLE;
HWREG(SOC_CM_PER_REGS + CM_PER_SPI0_CLKCTRL) = regVal;
McSPIReset(SPI_BASE);
/* Enable chip select pin.*/
McSPICSEnable(SPI_BASE); //CS use
/* Enable master mode of operation.*/
McSPIMasterModeEnable(SPI_BASE); //Master Mode
/* Perform the necessary configuration for master mode.*/
retVal = McSPIMasterModeConfig(SPI_BASE, MCSPI_MULTI_CH, MCSPI_TX_RX_MODE,\
MCSPI_DATA_LINE_COMM_MODE_1, SPI_CHAN);
McSPIClkConfig(SPI_BASE, MCSPI_IN_CLK, MCSPI_OUT_CLK,SPI_CHAN, MCSPI_CLK_MODE_0);
/* Configure the word length.*/
McSPIWordLengthSet(SPI_BASE, MCSPI_WORD_LENGTH(8), SPI_CHAN);
/* Set polarity of SPIEN to low.*/
McSPICSPolarityConfig(SPI_BASE, MCSPI_CS_POL_LOW, SPI_CHAN);
/* Enable the transmitter FIFO of McSPI peripheral.*/
McSPITxFIFOConfig(SPI_BASE, MCSPI_TX_FIFO_ENABLE, SPI_CHAN);
/* Enable the receiver FIFO of McSPI peripheral.*/
McSPIRxFIFOConfig(SPI_BASE, MCSPI_RX_FIFO_ENABLE, SPI_CHAN);
}
unsigned char McSPI_TxRx(unsigned char tx)
{
while(MCSPI_INT_TX_EMPTY(SPI_CHAN) != (McSPIIntStatusGet(SPI_BASE) & MCSPI_INT_TX_EMPTY(SPI_CHAN)));
McSPITransmitData(SPI_BASE, tx, SPI_CHAN);
while(MCSPI_INT_RX_FULL(SPI_CHAN) != (McSPIIntStatusGet(SPI_BASE) & MCSPI_INT_RX_FULL(SPI_CHAN)));
return McSPIReceiveData(SPI_BASE, SPI_CHAN);
}
unsigned int SPI_Read(unsigned int addr)
{
unsigned int ret=0;
//McSPICSAssert(SPI_BASE, SPI_CHAN);
McSPIChannelEnable(SPI_BASE, SPI_CHAN);
McSPI_TxRx(0x03);
McSPI_TxRx((addr & 0x00FF0000)>> 16);
McSPI_TxRx((addr & 0x0000FF00)>> 8);
McSPI_TxRx(addr & 0x000000FF);
ret = McSPI_TxRx(0x00);
ret |= McSPI_TxRx(0x00) << 8;
ret |= McSPI_TxRx(0x00) << 16;
ret |= McSPI_TxRx(0x00) << 24;
// McSPICSDeAssert(SPI_BASE, SPI_CHAN);
McSPIChannelDisable(SPI_BASE, SPI_CHAN);
return ret;
}
//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
But When Code Execute, Has not been asserted to Low SPI_CS0 when using multi channel mode,
How to implement SPIEN(SPI0_CS0,SPI0_CS1) in the Multi-Channel Mode ??