Hello All,
I am trying to get android working on a custom board with ICS with the latest release, I get this error during bootup.
Can anyone tell me where to look. Why this error occurs. I see PVR Crashes during bootup and i dont know why it is crashing.
Any pointers where should i look. How do i debug this issue. I am using PVR binaries that comes with ICS1.7.
Thanks.
--------- beginning of /dev/log/main
I/DEBUG ( 97): debuggerd: Oct 30 2012 17:17:30
F/libc ( 94): Fatal signal 11 (SIGSEGV) at 0x0000000c (code=1)
E/uim-sysfs( 95): uim: Inside main
E/uim-sysfs( 95): uim:BT/FM/GPS would be unavailable on system
I/Netd ( 96): Netd 1.0 starting
--------- beginning of /dev/log/system
I/Vold ( 93): Vold 2.1 (the revenge) firing up
D/Vold ( 93): Volume sdcard state changing -1 (Initializing) -> 0 (No-Media)
I/DEBUG ( 97): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
I/DEBUG ( 97): Build fingerprint: 'Android/full_blaze/blaze:4.0.4/IMM76L/eng.build.20121030.170732:eng/test-keys'
I/DEBUG ( 97): pid: 94, tid: 94 >>> /vendor/bin/pvrsrvinit <<<
I/DEBUG ( 97): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 0000000c
I/DEBUG ( 97): r0 00000000 r1 4004365c r2 400491ac r3 ffffff20
I/DEBUG ( 97): r4 beb7cc50 r5 00000000 r6 00000001 r7 beb7cc9c
I/DEBUG ( 97): r8 00000000 r9 00000000 10 00000000 fp 00000000
I/DEBUG ( 97): ip 0000a144 sp beb7ca90 lr 00008a14 pc 40019b8c cpsr 60000130
I/DEBUG ( 97): d0 7379732f206e656d d1 705f6472616f6269
I/DEBUG ( 97): d2 6569747265706f6c d3 61662f636f732f79
I/DEBUG ( 97): d4 0000000000000000 d5 0000000000000000
I/DEBUG ( 97): d6 0000000000000000 d7 018367cf00000000
I/DEBUG ( 97): d8 0000000000000000 d9 0000000000000000
I/DEBUG ( 97): d10 0000000000000000 d11 0000000000000000
I/DEBUG ( 97): d12 0000000000000000 d13 0000000000000000
I/DEBUG ( 97): d14 0000000000000000 d15 0000000000000000
I/DEBUG ( 97): d16 4178367cf91eb852 d17 3f50624dd2f1a9fc
I/DEBUG ( 97): d18 41b72fc8d2000000 d19 0000000000000000
I/DEBUG ( 97): d20 0000000000000000 d21 0000000000000000
I/DEBUG ( 97): d22 0000000000000000 d23 0000000000000000
I/DEBUG ( 97): d24 0000000000000000 d25 0000000000000000
I/DEBUG ( 97): d26 0000000000000000 d27 0000000000000000
I/DEBUG ( 97): d28 0000000000000000 d29 0000000000000000
I/DEBUG ( 97): d30 0000000000000000 d31 0000000000000000
I/DEBUG ( 97): scr 00000010
I/DEBUG ( 97):
I/DEBUG ( 97): #00 pc 00019b8c /system/lib/libc.so (clearerr)
I/DEBUG ( 97): #01 lr 00008a14 /system/vendor/bin/pvrsrvinit
I/DEBUG ( 97):
I/DEBUG ( 97): code around pc:
I/DEBUG ( 97): 40019b6c 6812447a 0c60f023 c00cf8a4 b1116811 zD.h#.`......h..
I/DEBUG ( 97): 40019b7c f0004620 bd10fb9f 0002991e 0002990c F..............
I/DEBUG ( 97): 40019b8c 300cf9b0 4604b570 f7f9b933 f04ffa53 ...0p..F3...S.O.
I/DEBUG ( 97): 40019b9c 210935ff e03e6001 447a4a20 68106812 .5.!.`>. JzD.h.h
I/DEBUG ( 97): 40019bac 4620b110 fbbaf000 f01589a5 d0030508 .. F............
I/DEBUG ( 97):
I/DEBUG ( 97): code around lr:
I/DEBUG ( 97): 000089f4 e3530e22 a3a03003 a5843014 ea000004 ".S..0...0......
I/DEBUG ( 97): 00008a04 e59f0044 ebffff23 e1a00005 ebffff48 D...#.......H...
I/DEBUG ( 97): 00008a14 e3a00000 e28dd044 e8bd80f0 00008fc6 ....D...........
I/DEBUG ( 97): 00008a24 00008db9 00008dad 00008dda 00008de1 ................
I/DEBUG ( 97): 00008a34 00008dfb 00008e34 00008e28 00008e57 ....4...(...W...
I/DEBUG ( 97):
I/DEBUG ( 97): stack:
I/DEBUG ( 97): beb7ca50 00000000
I/DEBUG ( 97): beb7ca54 00000000
I/DEBUG ( 97): beb7ca58 00000000
I/DEBUG ( 97): beb7ca5c 4001b601 /system/lib/libc.so
I/DEBUG ( 97): beb7ca60 00008db9 /system/vendor/bin/pvrsrvinit
I/DEBUG ( 97): beb7ca64 00008dfb /system/vendor/bin/pvrsrvinit
I/DEBUG ( 97): beb7ca68 0000002c
I/DEBUG ( 97): beb7ca6c 4003a24b /system/lib/libc.so
I/DEBUG ( 97): beb7ca70 00000001
I/DEBUG ( 97): beb7ca74 beb7ca64 [stack]
I/DEBUG ( 97): beb7ca78 00000002
I/DEBUG ( 97): beb7ca7c 00000000
I/DEBUG ( 97): beb7ca80 beb7cc50 [stack]
I/DEBUG ( 97): beb7ca84 00000000
I/DEBUG ( 97): beb7ca88 df0027ad
I/DEBUG ( 97): beb7ca8c 00000000
I/DEBUG ( 97): #00 beb7ca90 400487b4
I/DEBUG ( 97): beb7ca94 00000004
I/DEBUG ( 97): beb7ca98 00008f41 /system/vendor/bin/pvrsrvinit
I/DEBUG ( 97): beb7ca9c beb7cc9c [stack]
I/DEBUG ( 97): beb7caa0 4004370c /system/lib/libc.so
I/DEBUG ( 97): beb7caa4 00000000
I/DEBUG ( 97): beb7caa8 400487b4
I/DEBUG ( 97): beb7caac 40026337 /system/lib/libc.so
I/DEBUG ( 97): beb7cab0 400487b4
I/DEBUG ( 97): beb7cab4 40018a15 /system/lib/libc.so
I/DEBUG ( 97): beb7cab8 00008f41 /system/vendor/bin/pvrsrvinit
I/DEBUG ( 97): beb7cabc 00000000
I/DEBUG ( 97): beb7cac0 4001a3b9 /system/lib/libc.so
I/DEBUG ( 97): beb7cac4 00000000
I/DEBUG ( 97): beb7cac8 000001b6
I/DEBUG ( 97): beb7cacc 400486c4
I/DEBUG ( 97): beb7cad0 00008f41 /system/vendor/bin/pvrsrvinit
I/DEBUG ( 97): beb7cad4 beb7cc50 [stack]
I/ ( 101): ServiceManager: 0x66b910