This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Syslink integration with CCSV5



I notice that the syslink 2.20 directory that I have has a packages/ti directory structure which is typically used for CCS plugins.  Yet when I point CCS to that directory, it fails to find any RTSC products.  Is there a current repository for syslink, or are there any plans on integrating syslink into CCS anytime soon?

Thank you,

Michael

  • Syslink does not yet support the plugin required to be "discovered" by CCS. 

    In general, you could go to Windows->Preferences->CCS->RTSC ->Add -> Select Repository from File System 

    And then explicitly add <syslink _ installation>/packages to add it to the XDCPATH.