This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SATA power

Hello, I'm not using SATA on our OMAP application.

The PCB is designed for R1 silicon, meaning SATA_VDD is connected to 1.2V. For R2 and later, I can unconnect this. However the datasheet only states that I'll save: "additional power savings". How much power savings can I expect?

Likewise, I have connected SATA_VDDR to power. How much power savings can I expect if I remove this connection?

Thanks - I don't have good information on SATA power usage from the power estimation spreadsheet.

Gunter

 

 

 

  • Hi Gunter

    I believe the power savings on keeping these pins connected vs no connect would be in the order of 2-3 mW total.

    If you choose to keep these pins connected for continuity in design, just make sure that the peripheral is clock gated via PSC and the SATA PHY/PLL is powered down completely, which I think is the case by default.

    Hope this helps.

    Regards

    Mukul