This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

strange behaviour of EMIF Nor flash in No boot mode and in Nor boot mode

Other Parts Discussed in Thread: TMS320C6678

Hi

We developed our custom board with TMS320C6678 with I2c EEPROM (same IC used in EVM 6678) and with EMIF NOR Flash.

Without programming IBL in EPROM, If I connect emulator, put board either in no boot mode or in nor boot mode If I try to read device id / write /erase EMIF NOR flash its working perfectly ( we modified the platform driver to suite our EMIF Nor flash and its working ).

After Programming the IBL , I can able to read / write / erase flash only if i keep the board in No boot mode

If I keep the board in nor boot mode ( after programming IBL in eeprom) even the device id of nor flash read  through the emulator is wrong .

why this behaviour occurs ?

Please suggest

Thanks