Other Parts Discussed in Thread: 4460
Hi,
I'm trying to paly the video using H/w accelerators in jelly bean using panda board ES(omap 4460)
but it was loading ducati after DOMX error(D/DOMX ( 817): ERROR: failed check:(eError == OMX_ErrorNone) || (eError == OMX_ErrorNoMore) - returning error: 0x8000101a - Error returned from OMX API in ducati) was occuering.
Then video was playing using the software decoder.
please help me how to play the video using h/w decoder.
I'm attaching the logs.
I/ActivityManager( 269): START {act=android.intent.action.VIEW dat=content://media/external/video/media/22 typ=video/* cmp=com.android.gallery3d/.app.MovieActivity (8
W/OrientationEventListener( 798): Cannot detect sensors. Invalid disable
I/InputDispatcher( 269): Dropping event because there is no touched window.
W/BlobCache( 798): cannot read header
D/dalvikvm( 798): GC_CONCURRENT freed 4214K, 38% free 7178K/11564K, paused 15ms+7ms, total 61ms
D/dalvikvm( 798): WAIT_FOR_CONCURRENT_GC blocked 25ms
I/AudioService( 269): AudioFocus requestAudioFocus() from android.media.AudioManager@410ba330
I/ActivityManager( 269): Displayed com.android.gallery3d/.app.MovieActivity: +300ms
V/StateManager( 798): saveState
V/StateManager( 798): saveState class com.android.gallery3d.app.AlbumSetPage
V/StateManager( 798): saveState class com.android.gallery3d.app.AlbumPage
V/StateManager( 798): saveState class com.android.gallery3d.app.PhotoPage
E/WVMExtractor( 817): Failed to open libwvm.so
E/Trace ( 817): error opening trace file: No such file or directory (2)
[ 206.836364] rpmsg_omx rpmsg-omx1: local addr assigned: 0x401
[ 206.843139] omap-iommu omap-iommu.0: iommu_get: ducati qos_request
[ 206.869781] omap_hwmod: ipu: failed to hardreset
[ 206.878723] omap-iommu omap-iommu.0: ducati: version 2.1
[ 207.083923] rpmsg_omx rpmsg6: conn rsp: status 0 addr 101
D/DOMX ( 817): ERROR: failed check:(eError == OMX_ErrorNone) || (eError == OMX_ErrorNoMore) - returning error: 0x8000101a - Error returned from OMX API in ducati
D/DOMX ( 817): ERROR: failed check:eError == OMX_ErrorNone - returning error: 0x8000101a - Error in Proxy SetParameter for Enhanced port reconfig usage
I/OMXCodec( 817): [OMX.google.mpeg4.decoder] video dimensions are 352 x 288
I/OMXCodec( 817): [OMX.google.mpeg4.decoder] Crop rect is 352 x 288 @ (0, 0)
D/MediaPlayer( 798): getMetadata
I/OMXCodec( 817): [OMX.google.mpeg4.decoder] video dimensions are 848 x 480
I/OMXCodec( 817): [OMX.google.mpeg4.decoder] Crop rect is 848 x 480 @ (0, 0)
I/OMXCodec( 817): [OMX.google.mpeg4.decoder] video dimensions are 848 x 480
I/OMXCodec( 817): [OMX.google.mpeg4.decoder] Crop rect is 848 x 480 @ (0, 0)
D/dalvikvm( 269): GC_CONCURRENT freed 407K, 23% free 7569K/9760K, paused 4ms+9ms, total 109ms
W/OrientationEventListener( 798): Cannot detect sensors. Not enabled
D/dalvikvm( 798): GC_CONCURRENT freed 908K, 42% free 6759K/11564K, paused 7ms+7ms, total 52ms
D/dalvikvm( 798): WAIT_FOR_CONCURRENT_GC blocked 32ms
D/dalvikvm( 798): GC_FOR_ALLOC freed 8K, 40% free 6951K/11564K, paused 34ms, total 35ms
I/dalvikvm-heap( 798): Grow heap (frag case) to 7.835MB for 926736-byte allocation
D/dalvikvm( 798): GC_FOR_ALLOC freed <1K, 33% free 7856K/11564K, paused 37ms, total 37ms
I/GalleryEGLConfigChooser( 798): Config chosen: R5 G6 B5 A0 D24 S8 ID7 CAVEAT12344
I/GLRootView( 798): GLObject has changed from com.google.android.gles_jni.GLImpl@41050488 to com.google.android.gles_jni.GLImpl@4129a188
I/GLRootView( 798): onSurfaceChanged: 1024x564, gl10: com.google.android.gles_jni.GLImpl@4129a188
D/dalvikvm( 798): GC_CONCURRENT freed 42K, 32% free 7877K/11564K, paused 2ms+4ms, total 73ms
I/GLRootView( 798): onSurfaceChanged: 1024x564, gl10: com.google.android.gles_jni.GLImpl@4129a188
D/dalvikvm( 798): GC_FOR_ALLOC freed 30K, 33% free 7857K/11564K, paused 48ms, total 50ms
I/dalvikvm-heap( 798): Grow heap (frag case) to 8.720MB for 926736-byte allocation
D/dalvikvm( 798): GC_FOR_ALLOC freed <1K, 25% free 8762K/11564K, paused 41ms, total 41ms
D/dalvikvm( 798): GC_CONCURRENT freed 1K, 25% free 8767K/11564K, paused 2ms+6ms, total 55ms
D/dalvikvm( 798): GC_FOR_ALLOC freed 5K, 17% free 9672K/11564K, paused 32ms, total 32ms
I/dalvikvm-heap( 798): Grow heap (frag case) to 10.493MB for 926736-byte allocation
D/dalvikvm( 798): GC_FOR_ALLOC freed <1K, 16% free 10577K/12472K, paused 33ms, total 33ms
I/AudioService( 269): AudioFocus abandonAudioFocus() from android.media.AudioManager@410ba330
D/dalvikvm( 798): GC_FOR_ALLOC freed 3K, 16% free 10577K/12472K, paused 29ms, total 29ms
I/dalvikvm-heap( 798): Grow heap (frag case) to 11.375MB for 926736-byte allocation
D/dalvikvm( 798): GC_FOR_ALLOC freed 4K, 15% free 11477K/13380K, paused 31ms, total 31ms
V/StateManager( 798): finishState com.android.gallery3d.app.PhotoPage@410c2be0
I/GLRootView( 798): layout content pane 1024x564 (compensation 0)
V/StateManager( 798): finishState com.android.gallery3d.app.AlbumPage@4103b4c0
D/Gallery.MultiSetSync( 798): onSyncDone: MTP devices #pending=2
D/Gallery.MultiSetSync( 798): request sync: MTP devices
D/Gallery.MultiSetSync( 798): onSyncDone: Local albums #pending=1
D/Gallery.MultiSetSync( 798): request sync: Local albums
D/Gallery.MultiSetSync( 798): onSyncDone: picasa #pending=0
D/Gallery.MultiSetSync( 798): request sync: picasa
I/GLRootView( 798): layout content pane 1024x564 (compensation 0)
V/MtpDeviceSet( 798): loadDevices: [], size=0
with regards
v