This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sitara is not sending bootp request with SYSBOOT[4:0] as 10101 .

I am using Sitara(AM35xx) based Beagle bone board.

I have configured SYSBOOT pins using SYSBOOT[4:0] as 10101.

I have read the value of SYSBOOT pins upon power-on using SDCard bootup.

The value of control_status register (offset=0x40) is 0x00400315.

Next , I removed SD card(upon power-off).

Then, I restarted Beagle bone board.

Now, when I connect my Linux Laptop to the Beagle bone board using direct cable.

In wireshark window , I dont see any BOOTP request from the target.

Please advise.