Hi,
I am trying to enable support of DSP core on BB. I followed this post
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/537/t/196279.aspx
where TI wrote, that syslink shlould be used because dslink is unsupported at this time. So for this, I follow the instruction for Syslink
http://processors.wiki.ti.com/index.php/SysLink_Install_Guide
After make syslink I got an error I don't know
CC [M] /home/a/ti-sdk-beagleboard-05.05.00.00/syslink_2_20_02_20/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/family/hlos/knl/omap3530/Platform.o
CC [M] /home/a/ti-sdk-beagleboard-05.05.00.00/syslink_2_20_02_20/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/family/hlos/knl/omap3530/Linux/Cache.o
CC [M] /home/a/ti-sdk-beagleboard-05.05.00.00/syslink_2_20_02_20/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/family/hlos/knl/omap3530/omap3530dsp/omap3530_hal.o
In file included from /home/a/ti-sdk-beagleboard-05.05.00.00/syslink_2_20_02_20/packages/ti/syslink/inc/knl/Linux/omap3530_hal_mmu_defs.h:65:0,
from /home/a/ti-sdk-beagleboard-05.05.00.00/syslink_2_20_02_20/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/family/hlos/knl/omap3530/omap3530dsp/omap3530_hal.c:64:
arch/arm/plat-omap/include/plat/iommu.h: In function 'dev_to_omap_iommu':
arch/arm/plat-omap/include/plat/iommu.h:135:46: error: dereferencing pointer to incomplete type
make[4]: *** [/home/a/ti-sdk-beagleboard-05.05.00.00/syslink_2_20_02_20/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/family/hlos/knl/omap3530/omap3530dsp/omap3530_hal.o] Error 1
make[3]: *** [_module_/home/a/ti-sdk-beagleboard-05.05.00.00/syslink_2_20_02_20/packages/ti/syslink/utils/hlos/knl/Linux] Error 2
make[3]: Leaving directory `/home/a/ti-sdk-beagleboard-05.05.00.00/board-support/linux-3.3.7-r115'
make[2]: *** [default] Error 2
make[2]: Leaving directory `/home/a/ti-sdk-beagleboard-05.05.00.00/syslink_2_20_02_20/packages/ti/syslink/utils/hlos/knl/Linux'
make[1]: *** [syslink-driver-linux] Error 2
make[1]: Leaving directory `/home/a/ti-sdk-beagleboard-05.05.00.00/syslink_2_20_02_20/packages'
make: *** [syslink-driver] Error 2
Then I checked another http://omappedia.org/wiki/Syslink_Project but here I got that error
make[1]: *** No rule to make target `arch/arm/mach-omap2/remoteproc3xxx.o', needed by `arch/arm/mach-omap2/built-in.
o'. Stop. make: *** [arch/arm/mach-omap2] Error 2
So the queston is. How to enable DSP calculation on BeagleBoard-xM? Is there a simple way? :)