Dear friends
I want develop a camera based on the platform of DM6437 + Micron`s MT9M033 sensor , also i want to used the DM6437`s H3A engine.
Accroding to the MT9M033` s datasheet ,the maximum output clock is 74.25 M; and the DM6437's " preview engine is capable of processing up to 75 Mpixels/second";
Dose the DM6437 is fast enough to recive the MT9m033`s raw data ?
is there other things i need consideration to ?