HI
i have custom B/D and testing Off-Chip HDMI1 port output .
i changed sii9922a to sii9134(sii9034 compatible) chip . because we can't received sii9022a chip from local FAE.
i setted silicon image hdmi transmitter to the "1080p 422 embedded sync signal".
but i can't see anything.
Pls is there any check point?
any advice will be appreciated.
i attached my driver.
/*
*
* Silicon Image SIL9034 HDMI driver.
*
*
*/
#include <linux/init.h>
#include <linux/module.h>
#include <linux/kernel.h>
#include <linux/i2c.h>
#include <linux/delay.h>
#include <linux/fs.h>
#include <linux/slab.h>
#include <linux/miscdevice.h>
#include <linux/spinlock.h>
#include <linux/interrupt.h>
#include <linux/kthread.h>
#include <linux/jiffies.h>
#include <linux/poll.h>
#include <linux/workqueue.h>
#include <linux/mm.h>
#include <asm/types.h>
#include <asm/uaccess.h>
#include <asm/io.h>
#include <asm/irq.h>
#include <asm/page.h>
#include <asm/pgtable.h>
#include "sii9034hdmi.h" /* Silicon Image 9034 register definition */
#if 1
#define sil9034_dbg(fmt, arg...) \
printk(KERN_INFO "%s:%d> " fmt, __func__, __LINE__ , ## arg)
#else
#define sil9034_dbg(fmt, arg...)
#endif
#define I2C_RETRY_SLEEP 200
#define I2C_RETRY_COUNT 3
#define MOD_DESC "Sil9034 HDMI Driver"
/* Si9034 use 2 i2c to control the chip 0x39 & 0x3A */
#define SLAVE_SIZE 2
#define TIMER_JIFFIES (1 * HZ)
/* Timer only could cause the kernel busy, we push it into schedule */
#define SIL9034_TIMER 1
#define SIL9034_SCHED 1
/* Silicon Image provide 2 slave address to control. */
static int slave_num = 0 ;
static unsigned short normal_i2c[] = {
TX_SLV0, TX_SLV1, I2C_CLIENT_END
};
/* Macro need by addr_data */
I2C_CLIENT_INSMOD;
/* video mapping struct */
typedef struct sil9034_video_mapping
{
u8 video_reg ;
u16 value ;
} sil9034_video_mapping ;
/* video mapping for 480p YCbCr 4:2:2 Separate Sync Input*/
sil9034_video_mapping sil9034_480p_setting[] =
{
{DE_CTRL_ADDR,(DE_GEN_ENABLE|0x70)},
{DE_DELAY_ADDR,0x7A},
{DE_TOP_ADDR,0x24},
{DE_CNTH_ADDR,0x2},
{DE_CNTL_ADDR,0xD0},
{DEL_H_ADDR,0x1},
{DEL_L_ADDR,0xE0},
{TX_VID_CTRL_ADDR,CSCSEL_BT709|SET_EXTN_12BIT},
{TX_VID_MODE_ADDR,UPSMP_ENABLE|CSC_ENABLE},
{0,0}
};
/* video mapping for 720p YCbCr 4:2:2 Separate Sync Input*/
sil9034_video_mapping sil9034_720p_422_sepsync_setting[] =
{
{DE_CTRL_ADDR,(DE_GEN_ENABLE|0x1)},
{DE_DELAY_ADDR,0x04},
{DE_TOP_ADDR,0x19},
{DE_CNTH_ADDR,0x5},
{DE_CNTL_ADDR,0x00},
{DEL_H_ADDR,0x2},
{DEL_L_ADDR,0xD0},
{TX_VID_CTRL_ADDR,CSCSEL_BT709|SET_EXTN_12BIT},
//{TX_VID_MODE_ADDR,UPSMP_ENABLE|CSC_ENABLE},
{TX_VID_MODE_ADDR, 0}, // kisung cho change
{0,0}
};
/* video mapping for 720p YCbCr 4:2:2 Embedded Sync Input*/
sil9034_video_mapping sil9034_720p_422_embsync_setting[] =
{
{DE_CTRL_ADDR,0x0},
{DE_DELAY_ADDR,0x0},
{DE_TOP_ADDR,0x0},
{DE_CNTH_ADDR,0x0},
{DE_CNTL_ADDR,0x0},
{DEL_H_ADDR,0x0},
{DEL_L_ADDR,0x0},
{HBIT_TO_HSYNC_ADDR1,0x6E},
{HBIT_TO_HSYNC_ADDR2,0x0},
{HLENGTH1_ADDR,0x28},
{HLENGTH2_ADDR,0x0},
{VBIT_TO_VSYNC_ADDR,0x05},
{VLENGTH_ADDR,0x05},
{TX_VID_CTRL_ADDR,SET_EXTN_12BIT},
{TX_VID_MODE_ADDR,SYNCEXT_ENABLE},
{0,0}
};
/* video mapping for 1080i YCbCr 4:2:2 Separate Sync Input*/
sil9034_video_mapping sil9034_1080i_422_sepsync_setting[] =
{
{DE_CTRL_ADDR,(DE_GEN_ENABLE|0x0)},
{DE_DELAY_ADDR,0xC0},
{DE_TOP_ADDR,0x14},
{DE_CNTH_ADDR,0x07},
{DE_CNTL_ADDR,0x80},
{DEL_H_ADDR,0x2},
{DEL_L_ADDR,0x1C},
{TX_VID_CTRL_ADDR,CSCSEL_BT709|SET_EXTN_12BIT},
{TX_VID_MODE_ADDR,UPSMP_ENABLE|CSC_ENABLE},
{0,0}
};
/* video mapping for 1080P YCbCr 4:2:2 Embedded Sync Input*/
sil9034_video_mapping sil9034_1080p_422_embsync_setting[] =
{
{DE_CTRL_ADDR,(DE_GEN_ENABLE|0x0)},
{DE_DELAY_ADDR,0xC0},
{DE_TOP_ADDR,0x29},
{DE_CNTH_ADDR,0x07},
{DE_CNTL_ADDR,0x80},
{DEL_H_ADDR,0x4},
{DEL_L_ADDR,0x38},
{TX_VID_CTRL_ADDR,SET_EXTN_12BIT},
{TX_VID_MODE_ADDR,0},
{0,0}
};
/* i2c private data */
typedef struct davinci6446_sil9034
{
struct i2c_client* sil9034_client[SLAVE_SIZE] ;
#ifdef SIL9034_SCHED
struct work_struct work;
#endif
#ifdef SIL9034_TIMER
struct timer_list timer ;
#endif
spinlock_t lock;
/* pointer to different setting according to system */
sil9034_video_mapping *sil9034_setting ;
unsigned char work_flag ;
unsigned char auth_state ;
u8 an_ksv_data[8] ;
char r0rx[2] ;
char r0tx[2] ;
} davinci6446_sil9034 ;
static davinci6446_sil9034 ds ;
static int sii9034_probe(struct i2c_client *client, const struct i2c_device_id *id)
{
struct i2c_client *pclient;
printk("[%s]enter\n", __func__);
if (!(pclient = kzalloc(sizeof(*client), GFP_KERNEL)))
{
sil9034_dbg("ERROR error returned from kzalloc");
return -ENOMEM;
}
memcpy(pclient, client, sizeof(struct i2c_client));
ds.sil9034_client[slave_num] = pclient;
slave_num++;
printk("[%s]leave\n", __func__);
return 0;
}
static int sii9034_remove(struct i2c_client *client)
{
printk("[%s]enter\n", __func__);
printk("[%s]leave\n", __func__);
return 0;
}
static int sii9034_detect(struct i2c_client *client, struct i2c_board_info *info)
{
struct i2c_adapter *adapter = client->adapter;
printk("[%s]enter\n", __func__);
/* Jchen: i use a little trick here to make it register 2 i2c in 1 driver */
if (!i2c_check_functionality(adapter, I2C_FUNC_SMBUS_WRITE_BYTE))
{
sil9034_dbg("ERROR returned from i2c_check_functionality");
return -1;
}
printk( "chip found @ 0x%02x (%s)\n", client->addr << 1, client->adapter->name);
strlcpy(info->type, "sii9034", I2C_NAME_SIZE);
printk("[%s]leave\n", __func__);
return 0;
}
static const struct i2c_device_id sii9034_id[] = {
{ "sii9034", 0 },
{ }
};
MODULE_DEVICE_TABLE(i2c, sii9034_id);
static struct i2c_driver sil9034_driver = {
.class = I2C_CLASS_HWMON,
.driver = {
.owner = THIS_MODULE,
.name = "SIL9034 HDMI Driver",
},
.probe = sii9034_probe,
.remove = sii9034_remove,
.detect = sii9034_detect,
//.attach_adapter = &sil9034_attach_adapter,
//.detach_client = &sil9034_detach_client,
.id_table = sii9034_id, /*define in i2c-id.h */
.address_list = normal_i2c,
};
static const char * pname = "SIL9034 HDMI Driver" ;
#if 0
static int sil9034_detect_client(struct i2c_adapter * adapter, int address, int kind)
{
int ret = 0;
struct i2c_client* client = NULL;
/* Jchen: i use a little trick here to make it register 2 i2c in 1 driver */
if (!i2c_check_functionality(adapter, I2C_FUNC_SMBUS_WRITE_BYTE))
{
sil9034_dbg("ERROR returned from i2c_check_functionality");
ret = -1;
goto out;
}
if (!(client = kzalloc(sizeof(*client), GFP_KERNEL)))
{
sil9034_dbg("ERROR error returned from kzalloc");
ret = -ENOMEM;
goto out;
}
memset(client, 0, sizeof(struct i2c_client));
client->addr = address;
client->adapter = adapter;
client->driver = &sil9034_driver;
/* Jchen: it seem like ten bit probe doesn't support here, but we don't need
* it, since we know that the i2c address is fix in embedded.
* client->flags = I2C_M_IGNORE_NAK|I2C_M_TEN;
*/
client->flags = I2C_M_IGNORE_NAK;
strcpy(client->name, "sil9034");
/* JChen: i use force mode, no need this */
if ((ret = i2c_attach_client(client)) != 0)
{
sil9034_dbg("%s Unable to attach client.\n", pname);
kfree(client);
ret = -1;
goto out;
}
ds.sil9034_client[slave_num++] = client;
out:
return ret;
}
static int sil9034_attach_adapter(struct i2c_adapter * adapter)
{
/* JChen : force to support 10-bit address, i2c-core need to
* fix to follow the linux i2c game.
sil9034_detect_client(adapter,TX_SLV0,I2C_DRIVERID_SIL9034) ;
sil9034_detect_client(adapter,TX_SLV1,I2C_DRIVERID_SIL9034) ;
*/
return(i2c_probe(adapter, &addr_data, &sil9034_detect_client));
}
static int sil9034_detach_client(struct i2c_client * client)
{
int ret = 0;
if ((ret = i2c_detach_client(client)) != 0)
{
sil9034_dbg("%s Unable to detach client.\n", pname);
goto out;
}
#if SIL9034_TIMER
del_timer_sync(&ds.timer);
#endif
#if SIL9034_SCHED
flush_scheduled_work();
#endif
kfree(client);
out:
return ret;
}
#endif
static int sil9034_write(davinci6446_sil9034 *priv,u8 slave,u8 reg, u16 value)
{
int retry = I2C_RETRY_COUNT;
struct i2c_client* client;
int ret = -1;
if(slave > 1) {
printk("[%s]ERROR slave index :%d\n", __func__, slave);
return -1;
}
client = priv->sil9034_client[slave];
if(!client) return 0xff;
while(retry--)
{
ret = i2c_smbus_write_byte_data(client, reg, value);
if (-1 != ret) break;
printk("sil9034_write retry [%d]\n", retry);
mdelay(I2C_RETRY_SLEEP);
}
return ret;
}
/* JChen: this should be call by others driver or
* create new char dev to ioctl the control.
*/
EXPORT_SYMBOL(sil9034_write);
static int sil9034_read(davinci6446_sil9034 *priv,u8 slave,u8 reg)
{
int retry = I2C_RETRY_COUNT;
int dat;
struct i2c_client* client;
if(slave > 1) {
printk("[%s]ERROR slave index :%d\n", __func__, slave);
return -1;
}
client = priv->sil9034_client[slave];
if(!client) return 0xff;
while(retry--)
{
dat = i2c_smbus_read_byte_data(priv->sil9034_client[slave], reg);
if (-1 != dat) break;
printk("(sil9034_read) retry [%d]\n", retry);
mdelay(I2C_RETRY_SLEEP);
}
return dat;
}
EXPORT_SYMBOL(sil9034_read);
static char *sil9034_ddc_write(davinci6446_sil9034 *priv,u8 *value,u8 reg, u8 length)
{
u8 count = 0 ;
while(sil9034_read(priv,SLAVE0,DDC_STATUS_ADDR)&BIT_MDDC_ST_IN_PROGR)
mdelay(10) ;
sil9034_write(priv,SLAVE0,DDC_ADDR,HDCP_RX_SLAVE) ;
sil9034_write(priv,SLAVE0,DDC_OFFSET_ADDR,reg) ;
sil9034_write(priv,SLAVE0,DDC_CNT1_ADDR,length) ;
sil9034_write(priv,SLAVE0,DDC_CNT2_ADDR,0) ;
sil9034_write(priv,SLAVE0,DDC_CMD_ADDR,MASTER_CMD_CLEAR_FIFO) ;
for(count=0 ;count < length ; count++)
{
sil9034_write(priv,SLAVE0,DDC_DATA_ADDR,value[count]) ;
}
sil9034_write(priv,SLAVE0,DDC_CMD_ADDR,MASTER_CMD_SEQ_WR) ;
while(sil9034_read(priv,SLAVE0,DDC_STATUS_ADDR)&BIT_MDDC_ST_IN_PROGR)
mdelay(10) ;
sil9034_dbg("DDC WRITE FIFO is %d\n",sil9034_read(priv,SLAVE0,DDC_FIFOCNT_ADDR)) ;
sil9034_write(priv,SLAVE0,DDC_CMD_ADDR,MASTER_CMD_ABORT) ;
sil9034_write(priv,SLAVE0,DDC_CMD_ADDR,MASTER_CMD_CLOCK) ;
sil9034_write(priv,SLAVE0,DDC_MAN_ADDR,0) ;
return NULL ;
}
static char *sil9034_ddc_read(davinci6446_sil9034 *priv,u8 *value,u8 reg, u8 length)
{
u8 count = 0 ;
sil9034_write(priv,SLAVE0,DDC_ADDR,HDCP_RX_SLAVE) ;
sil9034_write(priv,SLAVE0,DDC_OFFSET_ADDR,reg) ;
sil9034_write(priv,SLAVE0,DDC_CNT1_ADDR,length) ;
sil9034_write(priv,SLAVE0,DDC_CNT2_ADDR,0) ;
sil9034_write(priv,SLAVE0,DDC_CMD_ADDR,MASTER_CMD_CLEAR_FIFO) ;
sil9034_write(priv,SLAVE0,DDC_CMD_ADDR,MASTER_CMD_SEQ_RD) ;
while(sil9034_read(priv,SLAVE0,DDC_STATUS_ADDR)&BIT_MDDC_ST_IN_PROGR)
mdelay(10) ;
sil9034_dbg("DDC READ FIFO is %d\n",sil9034_read(priv,SLAVE0,DDC_FIFOCNT_ADDR)) ;
for(count=0 ;count < length ; count++)
{
value[count] = sil9034_read(priv,SLAVE0,DDC_DATA_ADDR) ;
}
while(sil9034_read(priv,SLAVE0,DDC_STATUS_ADDR)&BIT_MDDC_ST_IN_PROGR)
mdelay(10) ;
sil9034_write(priv,SLAVE0,DDC_CMD_ADDR,MASTER_CMD_ABORT) ;
sil9034_write(priv,SLAVE0,DDC_CMD_ADDR,MASTER_CMD_CLOCK) ;
sil9034_write(priv,SLAVE0,DDC_MAN_ADDR,0) ;
return NULL ;
}
//-------------------------- INIT / EXIT ---------------------------------------------------------
static int sil9034_chipInfo(davinci6446_sil9034 *priv)
{
u8 device_info[3] = {255,255,255} ;
device_info[1] = sil9034_read(priv,SLAVE0,DEV_IDL) ;
device_info[0] = sil9034_read(priv,SLAVE0,DEV_IDH) ;
device_info[2] = sil9034_read(priv,SLAVE0,DEV_REV) ;
printk(KERN_INFO "Silicon Image Device Driver Id 0x%02X%02X. Rev %02i.\n",device_info[0],device_info[1],device_info[2]) ;
return 0 ;
}
static int sil9034_audioInfoFrameSetting(davinci6446_sil9034 *priv)
{
u8 aud_info_addr ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
/* set the audio info frame type according to EIA-CEA-861-B datasheet */
aud_info_addr = AUD_IF_ADDR ;
/* Audio type , pg 78 on EIA_CEA_861_B.pdf */
sil9034_write(priv,SLAVE1,aud_info_addr++,0x04) ;
/* Audio version */
sil9034_write(priv,SLAVE1,aud_info_addr++,0x01) ;
/* Audio info frame length */
sil9034_write(priv,SLAVE1,aud_info_addr++,0x10) ;
/* Audio info frame chsum */
sil9034_write(priv,SLAVE1,aud_info_addr++,(0x04+0x01+0x10)) ;
/* AUDIO INFO DATA BYTE , according to Sil FAE, 5 byte is enought.
* page 56
*/
/* CT3 | CT2 | CT1 | CT0 | Rsvd | CC2 | CC1 | CC0| */
sil9034_write(priv,SLAVE1,aud_info_addr++,0x11) ;
/* Reserved (shall be 0) | SF2 | SF1 | SF0 | SS1 | SS0 |*/
/* I should provide ioctl to re-sampling the frequence according
* to audio header type in user space program.
*/
sil9034_write(priv,SLAVE1,aud_info_addr++,0x1D) ;
/* format depend on data byte 1 */
sil9034_write(priv,SLAVE1,aud_info_addr++,0x11) ;
/* CA7 | CA6 | CA5 | CA4 | CA3 | CA2 | CA1 | CA0 | */
sil9034_write(priv,SLAVE1,aud_info_addr++,0) ;
/* DM_I NH | LSV3 | LSV2 | LSV1 | LSV0 | Reserved (shall be 0)| */
sil9034_write(priv,SLAVE1,aud_info_addr++,0) ;
return 0 ;
}
static int sil9034_cea861InfoFrameControl1(davinci6446_sil9034 *priv,u8 enable)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
/* enable the avi repeat transmission */
reg_value = sil9034_read(priv,SLAVE1,INF_CTRL1) ;
if(enable)
sil9034_write(priv,SLAVE1,INF_CTRL1,(reg_value | (BIT_AVI_REPEAT |BIT_AUD_ENABLE |BIT_AUD_REPEAT))) ;
else
sil9034_write(priv,SLAVE1,INF_CTRL1,0) ;
reg_value = sil9034_read(priv,SLAVE1,INF_CTRL1) ;
sil9034_dbg("InfoFrame control#1 register 0x%x = 0x%x\n",INF_CTRL1,reg_value) ;
return 0 ;
}
static int sil9034_cea861InfoFrameControl2(davinci6446_sil9034 *priv,u8 enable)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
/* Generic packet transmittion & repeat mode enable */
reg_value = sil9034_read(priv,SLAVE1,INF_CTRL2) ;
if(enable)
{
/* enable GCP_RPT , GCP_EN */
sil9034_write(priv,SLAVE1,INF_CTRL2,(reg_value |(GCP_EN|GCP_RPT))) ;
}
else
{
sil9034_write(priv,SLAVE1,INF_CTRL2,reg_value & ~(GCP_EN|GCP_RPT)) ;
}
reg_value = sil9034_read(priv,SLAVE1,INF_CTRL2) ;
sil9034_dbg("InfoFrame control#2 register 0x%x = 0x%x\n",INF_CTRL2,reg_value) ;
return 0 ;
}
static int sil9034_switchClock2M48X1(davinci6446_sil9034 *priv,u8 enable)
{
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
#if 0
outw((inw(IO_CLK_MOD2) & (~(0x1000))), IO_CLK_MOD2); /* disable I2C clock first */
outw((inw(IO_CLK_DIV4) | 0x01F | 0x0C00), IO_CLK_DIV4);
outw((inw(IO_CLK_MOD2) | 0x1000), IO_CLK_MOD2); /* re-enable I2C clock */
if(enable)
{
/* use M48X1 */
outw((inw(IO_CLK_SEL0) | 0x0000), IO_CLK_SEL0); /* select M48X1 */
}
else
{
/* Use PLLB, MSP430 need this */
outw((inw(IO_CLK_SEL0) | 0x0C00), IO_CLK_SEL0); /* select PLLB */
}
#endif
return 0 ;
}
static int sil9034_cea861InfoFrameSetting(davinci6446_sil9034 *priv)
{
u8 avi_info_addr ;
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
reg_value = sil9034_read(priv,SLAVE1,INF_CTRL1) ;
sil9034_write(priv,SLAVE1,INF_CTRL1,reg_value & (~BIT_AVI_REPEAT)) ;
mdelay(64) ; // Delay VSync for unlock DATA buffer
if(sil9034_read(priv,SLAVE1,INF_CTRL1)&BIT_AVI_ENABLE)
sil9034_dbg("Sent AVI error\n") ;
else
sil9034_dbg("Silicon Image sending AVI success.\n") ;
if(sil9034_read(priv,SLAVE1,INF_CTRL1)&BIT_AUD_ENABLE)
sil9034_dbg("Sent AUD error\n") ;
else
sil9034_dbg("Silicon Image sending AUD success.\n") ;
/* set the info frame type according to CEA-861 datasheet */
avi_info_addr = AVI_IF_ADDR ;
/* AVI type */
sil9034_write(priv,SLAVE1,avi_info_addr++,0x82) ;
/* AVI version */
sil9034_write(priv,SLAVE1,avi_info_addr++,0x02) ;
/* AVI length */
sil9034_write(priv,SLAVE1,avi_info_addr++,0x13) ;
/* AVI CRC */
sil9034_write(priv,SLAVE1,avi_info_addr++,(0x82 + 0x02 + 0x13 + 0x1D)) ;
/* AVI DATA BYTE , according to Sil FAE, 3 byte is enought.
* page 102
*/
/* 0 | Y1 | Y0 | A0 | B1 | B0 | S1 | S0 */
sil9034_write(priv,SLAVE1,avi_info_addr++,0x1D) ;
/* C1 | C0 | M1 | M0 | R3 | R2 | R1 | R0 */
sil9034_write(priv,SLAVE1,avi_info_addr++,0x68) ;
/* 0 | 0 | 0 | 0 | 0 | 0 | SC1 | SC0 */
sil9034_write(priv,SLAVE1,avi_info_addr++,0x3) ;
reg_value = sil9034_read(priv,SLAVE1,INF_CTRL1) ;
sil9034_write(priv,SLAVE1,INF_CTRL1,reg_value | (BIT_AVI_ENABLE|BIT_AVI_REPEAT)) ;
return 0 ;
}
static int sil9034_wakeupHdmiTx(davinci6446_sil9034 *priv)
{
u8 reg_value ;
reg_value = sil9034_read(priv,SLAVE0,TX_SYS_CTRL1_ADDR) ;
sil9034_write(priv,SLAVE0,TX_SYS_CTRL1_ADDR,reg_value|SET_PD) ;
sil9034_write(priv,SLAVE0,INT_CNTRL_ADDR,0) ;
reg_value = sil9034_read(priv,SLAVE1,INF_CTRL1) ;
sil9034_write(priv,SLAVE1,INF_CTRL1,reg_value |BIT_AVI_REPEAT|BIT_AUD_REPEAT) ;
return 0 ;
}
static int sil9034_sentCPPackage(davinci6446_sil9034 *priv,u8 enable)
{
u8 reg_value ;
u8 timeout = 64 ;
reg_value = sil9034_read(priv,SLAVE1,INF_CTRL2) ;
sil9034_write(priv,SLAVE1,INF_CTRL2,reg_value &~BIT_CP_REPEAT) ;
if(enable)
sil9034_write(priv,SLAVE1,CP_IF_ADDR,BIT_CP_AVI_MUTE_SET) ;
else
sil9034_write(priv,SLAVE1,CP_IF_ADDR,BIT_CP_AVI_MUTE_CLEAR) ;
while(timeout--)
{
if(!sil9034_read(priv,SLAVE1,INF_CTRL2)&BIT_CP_REPEAT)
break ;
}
if(timeout)
sil9034_write(priv,SLAVE1,INF_CTRL2,reg_value |(BIT_CP_REPEAT|BIT_CP_ENABLE)) ;
return 0 ;
}
int sil9034_unmaskInterruptStatus(davinci6446_sil9034 *priv)
{
u8 reg_value = 0xFF ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
sil9034_write(priv,SLAVE0,HDMI_INT1_MASK,reg_value) ;
sil9034_write(priv,SLAVE0,HDMI_INT2_MASK,reg_value) ;
sil9034_write(priv,SLAVE0,HDMI_INT3_MASK,reg_value) ;
return 0 ;
}
static int sil9034_hdmiOutputConfig(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
/* HDMI control register , enable HDMI, disable DVI */
reg_value = sil9034_read(priv,SLAVE1,HDMI_CTRL_ADDR) ;
sil9034_write(priv,SLAVE1,HDMI_CTRL_ADDR,(reg_value | HDMI_MODE_ENABLE)) ;
reg_value = sil9034_read(priv,SLAVE1,HDMI_CTRL_ADDR) ;
sil9034_dbg("Hdmi control register 0x%x = 0x%x\n",HDMI_CTRL_ADDR,reg_value) ;
return 0 ;
}
static int sil9034_ddcSetting(davinci6446_sil9034 *priv)
{
sil9034_write(priv,SLAVE0,DDC_ADDR,HDCP_RX_SLAVE) ;
return 0 ;
}
static int sil9034_powerDown(davinci6446_sil9034 *priv,u8 enable)
{
/* power down internal oscillator
* disable internal read of HDCP keys and KSV
* disable master DDC block
* page 4,50,113
*/
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
reg_value = sil9034_read(priv,SLAVE0,TX_SYS_CTRL1_ADDR) ;
if(enable)
{
sil9034_write(priv,SLAVE1,DIAG_PD_ADDR,~(0x7)) ;
sil9034_write(priv,SLAVE0,TX_SYS_CTRL1_ADDR,reg_value & ~0x1) ;
}
else
{
sil9034_write(priv,SLAVE1,DIAG_PD_ADDR,0x7) ;
sil9034_write(priv,SLAVE0,TX_SYS_CTRL1_ADDR,(reg_value | 0x1)) ;
}
reg_value = sil9034_read(priv,SLAVE0,TX_SYS_CTRL1_ADDR) ;
sil9034_dbg("System control register #1 0x%x = 0x%x\n",TX_SYS_CTRL1_ADDR, reg_value) ;
reg_value = sil9034_read(priv,SLAVE1,DIAG_PD_ADDR) ;
sil9034_dbg("Diagnostic power down register 0x%x = 0x%x\n",DIAG_PD_ADDR, reg_value) ;
return 0 ;
}
static int sil9034_swReset(davinci6446_sil9034 *priv)
{
/* use to temporary save inf_ctrl */
u8 temp1 ;
u8 temp2 ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
temp1 = sil9034_read(priv,SLAVE1,INF_CTRL1) ;
temp2 = sil9034_read(priv,SLAVE1,INF_CTRL2) ;
/*
* audio fifo reset enable
* software reset enable
*/
while(!sil9034_read(priv,SLAVE0,TX_STAT_ADDR)&P_STABLE)
mdelay(10) ;
sil9034_write(priv,SLAVE0,TX_SWRST_ADDR,(BIT_TX_SW_RST|BIT_TX_FIFO_RST)) ;
mdelay(10) ;
sil9034_write(priv,SLAVE0,TX_SWRST_ADDR,0) ;
mdelay(64) ; // allow TCLK (sent to Rx across the HDMS link) to stabilize
/* restore */
sil9034_write(priv,SLAVE1,INF_CTRL1,temp1) ;
sil9034_write(priv,SLAVE1,INF_CTRL2,temp2) ;
return 0 ;
}
static int sil9034_triggerRom(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
reg_value = sil9034_read(priv,SLAVE0,KEY_COMMAND_ADDR) ;
sil9034_write(priv,SLAVE0,KEY_COMMAND_ADDR,reg_value & ~LD_KSV) ;
mdelay(10) ;
sil9034_write(priv,SLAVE0,KEY_COMMAND_ADDR,reg_value |LD_KSV) ;
mdelay(10) ;
sil9034_write(priv,SLAVE0,KEY_COMMAND_ADDR,reg_value & ~LD_KSV) ;
return 0 ;
}
static int sil9034_generalControlPacket(davinci6446_sil9034 *priv,u8 enable)
{
u8 reg_value ;
/*
* mute the video & audio
*/
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
reg_value = sil9034_read(priv,SLAVE1,GCP_BYTE1) ;
if(enable)
{
/* set avmute flag */
sil9034_write(priv,SLAVE1,GCP_BYTE1,(reg_value | SET_AVMUTE)) ;
}
else
{
/* clear avmute flag */
sil9034_write(priv,SLAVE1,GCP_BYTE1,(reg_value | CLR_AVMUTE)) ;
}
reg_value = sil9034_read(priv,SLAVE1,GCP_BYTE1) ;
sil9034_dbg("General control packet register 0x%x = 0x%x\n",GCP_BYTE1,reg_value) ;
return 0 ;
}
static int sil9034_audioInputConfig(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
/* Audio mode register */
sil9034_write(priv,SLAVE1,AUD_MODE_ADDR,0xF9) ;
reg_value = sil9034_read(priv,SLAVE1,AUD_MODE_ADDR) ;
sil9034_dbg("Audio in mode register 0x%x = 0x%x\n",AUD_MODE_ADDR,reg_value) ;
/* ACR audio frequency register: * MCLK=128 Fs */
sil9034_write(priv,SLAVE1,FREQ_SVAL_ADDR,0) ;
reg_value = sil9034_read(priv,SLAVE1,FREQ_SVAL_ADDR) ;
sil9034_dbg("Audio frequency register 0x%x = 0x%x\n",FREQ_SVAL_ADDR,reg_value) ;
return 0 ;
}
static int sil9034_hdmiVideoEmbSyncDec(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
reg_value = sil9034_read(priv,SLAVE0,INTERLACE_ADJ_MODE) ;
sil9034_write(priv,SLAVE0,INTERLACE_ADJ_MODE,(reg_value & ~(0x7))) ;
reg_value = sil9034_read(priv,SLAVE0,INTERLACE_ADJ_MODE) ;
sil9034_dbg("Interlace Adjustment register 0x%x = 0x%x\n",INTERLACE_ADJ_MODE,reg_value) ;
return 0 ;
}
static int sil9034_hdmiTmdsConfig(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
/* TMDS control register
* FPLL is 1.0*IDCK.
* Internal source termination enabled.
* Driver level shifter bias enabled.
* page 27
*/
reg_value = sil9034_read(priv,SLAVE0,TX_TMDS_CTRL_ADDR) ;
sil9034_write(priv,SLAVE0,TX_TMDS_CTRL_ADDR,reg_value|0x5) ;
reg_value = sil9034_read(priv,SLAVE0,TX_TMDS_CTRL_ADDR) ;
sil9034_dbg("TMDS control register 0x%x = 0x%x\n",TX_TMDS_CTRL_ADDR,reg_value) ;
}
static int sil9034_hdmiHdcpConfig(davinci6446_sil9034 *priv,u8 enable)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
/* HDMI HDCP configuration */
reg_value = sil9034_read(priv,SLAVE0,HDCP_CTRL_ADDR) ;
if(enable){
sil9034_write(priv,SLAVE0,HDCP_CTRL_ADDR,(reg_value | SET_ENC_EN)) ;
priv->auth_state = AUTH_NEED ;
}else{
sil9034_write(priv,SLAVE0,HDCP_CTRL_ADDR,(reg_value & ~(SET_ENC_EN))) ;
priv->auth_state = AUTH_DONE ;
}
reg_value = sil9034_read(priv,SLAVE0,HDCP_CTRL_ADDR) ;
sil9034_dbg("Hdmi hdcp register 0x%x = 0x%x\n",HDCP_CTRL_ADDR,reg_value) ;
return 0 ;
}
char sil9034_hotplugEvent(davinci6446_sil9034 *priv)
{
u8 reg_value ;
reg_value = sil9034_read(priv,SLAVE0,TX_STAT_ADDR) ;
if(reg_value&SET_HPD)
return 1 ;
else
return 0 ;
}
static int sil9034_checkHdcpDevice(davinci6446_sil9034 *priv)
{
u8 total = 0 ;
u8 bits = 0 ;
u8 count = 0 ;
/* read 5 byte from ddc */
sil9034_ddc_read(priv,&priv->an_ksv_data[0],DDC_BKSV_ADDR,5) ;
/* calculate bits */
for(count=0 ;count<5 ; count++)
{
sil9034_dbg("bksv %d,0x%x\n",count,priv->an_ksv_data[count]) ;
for(bits=0 ;bits<8 ; bits++)
if(priv->an_ksv_data[count] & (1<<bits))
total++ ;
}
if(total == HDCP_ACC)
return TRUE ;
else
return FALSE ;
}
static int sil9034_toggleRepeatBit(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
reg_value = sil9034_read(priv,SLAVE0,HDCP_CTRL_ADDR) ;
if(reg_value & RX_RPTR_ENABLE)
sil9034_write(priv,SLAVE0,HDCP_CTRL_ADDR,reg_value&~RX_RPTR_ENABLE) ;
else
sil9034_write(priv,SLAVE0,HDCP_CTRL_ADDR,reg_value|RX_RPTR_ENABLE) ;
return 0 ;
}
static int sil9034_releaseCPReset(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
reg_value = sil9034_read(priv,SLAVE0,HDCP_CTRL_ADDR) ;
sil9034_write(priv,SLAVE0,HDCP_CTRL_ADDR,reg_value|SET_CP_RESTN) ;
return 0 ;
}
static int sil9034_StopRepeatBit(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
reg_value = sil9034_read(priv,SLAVE0,HDCP_CTRL_ADDR) ;
sil9034_write(priv,SLAVE0,HDCP_CTRL_ADDR,reg_value&~RX_RPTR_ENABLE) ;
return 0 ;
}
static int sil9034_writeAnHdcpRx(davinci6446_sil9034 *priv)
{
/* write 8 byte to ddc hdcp rx*/
sil9034_ddc_write(priv,&priv->an_ksv_data[0],DDC_AN_ADDR,8) ;
return 0 ;
}
static int sil9034_writeBksvHdcpTx(davinci6446_sil9034 *priv)
{
u8 count = 0 ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
for(count=0; count<5; count++)
{
sil9034_write(priv,SLAVE0,HDCP_BKSV1_ADDR+count,priv->an_ksv_data[count]) ;
sil9034_dbg("write bksv to tx 0x%x\n",priv->an_ksv_data[count]) ;
}
return 0 ;
}
static int sil9034_readBksvHdcpRx(davinci6446_sil9034 *priv)
{
u8 count = 0 ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
/* read 5 byte from ddc */
sil9034_ddc_read(priv,&priv->an_ksv_data[0],DDC_BKSV_ADDR,5) ;
for(count=0; count<5; count++)
{
sil9034_dbg("bksv data %d 0x%x\n",count,priv->an_ksv_data[count]) ;
}
return 0 ;
}
static int sil9034_writeAksvHdcpRx(davinci6446_sil9034 *priv)
{
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
/* write 5 byte to ddc hdcp rx*/
sil9034_ddc_write(priv,&priv->an_ksv_data[0],DDC_AKSV_ADDR,5) ;
return 0 ;
}
static int sil9034_readAksvHdcpTx(davinci6446_sil9034 *priv)
{
u8 count = 0 ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
for(count=0; count<5; count++)
{
priv->an_ksv_data[count] = sil9034_read(priv,SLAVE0,HDCP_AKSV1_ADDR+count) ;
sil9034_dbg("aksv data %d 0x%x\n",count,priv->an_ksv_data[count]) ;
}
return 0 ;
}
static int sil9034_readAnHdcpTx(davinci6446_sil9034 *priv)
{
u8 count = 0 ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
for(count=0; count<8; count++)
{
priv->an_ksv_data[count] = sil9034_read(priv,SLAVE0,HDCP_AN1_ADDR+count) ;
sil9034_dbg("an data %d 0x%x\n",count,priv->an_ksv_data[count]) ;
}
return 0 ;
}
static int sil9034_generateAn(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
reg_value = sil9034_read(priv,SLAVE0,HDCP_CTRL_ADDR) ;
sil9034_write(priv,SLAVE0,HDCP_CTRL_ADDR,reg_value&~TX_ANSTOP) ;
mdelay(10) ;
sil9034_write(priv,SLAVE0,HDCP_CTRL_ADDR,reg_value|TX_ANSTOP) ;
return 0 ;
}
static int sil9034_isRepeater(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
/* read 1 byte from ddc */
sil9034_ddc_read(priv,®_value,DDC_BCAPS_ADDR,1) ;
if(reg_value&DDC_BIT_REPEATER)
return TRUE ;
return FALSE ;
}
static int sil9034_compareR0(davinci6446_sil9034 *priv)
{
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
/* read 2 byte from ddc */
sil9034_ddc_read(priv,&priv->r0rx[0],DDC_RI_ADDR,2) ;
priv->r0tx[0] = sil9034_read(priv,SLAVE0,HDCP_RI1) ;
priv->r0tx[1] = sil9034_read(priv,SLAVE0,HDCP_RI2) ;
if((priv->r0rx[0]==priv->r0tx[0])&&(priv->r0rx[1]==priv->r0tx[1]))
{
printk(KERN_INFO "HDCP handshake complete match.\n") ;
return TRUE ;
}
return FALSE ;
}
static int sil9034_videoInputConfig(davinci6446_sil9034 *priv)
{
u8 count = 0 ;
/* Auto setting by the sil9034_video_mapping struct */
while(priv->sil9034_setting[count++].video_reg != 0)
{
sil9034_dbg("setting count %d 0x%x-0x%x\n",count,\
priv->sil9034_setting[count].video_reg,\
priv->sil9034_setting[count].value) ;
sil9034_write(priv,SLAVE0,priv->sil9034_setting[count].video_reg,\
priv->sil9034_setting[count].value) ;
}
return 0 ;
}
static int sil9034_autoRiCheck(davinci6446_sil9034 *priv,u8 enable)
{
u8 reg_value ;
reg_value = sil9034_read(priv,SLAVE0,RI_CMD_ADDR) ;
if(enable)
sil9034_write(priv,SLAVE0,RI_CMD_ADDR, reg_value|SET_RI_ENABLE);
else
sil9034_write(priv,SLAVE0,RI_CMD_ADDR, reg_value&~SET_RI_ENABLE);
return 0 ;
}
int sil9034_dumpSystemStatus(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
reg_value = sil9034_read(priv,SLAVE0,TX_STAT_ADDR) ;
sil9034_dbg("System status register 0x%x = 0x%x\n",TX_STAT_ADDR,reg_value) ;
return 0 ;
}
int sil9034_dumpDataCtrlStatus(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
reg_value = sil9034_read(priv,SLAVE0,DCTL_ADDR) ;
sil9034_dbg("Data control register 0x%x = 0x%x\n",DCTL_ADDR,reg_value) ;
return 0 ;
}
int sil9034_clearInterruptStatus(davinci6446_sil9034 *priv)
{
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
/*
u8 reg_value ;
reg_value = sil9034_read(priv,SLAVE0,INT_CNTRL_ADDR) ;
sil9034_write(priv,SLAVE0,INT_CNTRL_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,INT_CNTRL_ADDR) ;
sil9034_dbg("Interrupt control register 0x%x = 0x%x\n",INT_CNTRL_ADDR,reg_value) ;
*/
sil9034_write(priv,SLAVE0,INT_SOURCE1_ADDR,0xFF) ;
sil9034_write(priv,SLAVE0,INT_SOURCE2_ADDR,0xFF) ;
sil9034_write(priv,SLAVE0,INT_SOURCE3_ADDR,0xFF) ;
return 0 ;
}
int sil9034_dumpInterruptSourceStatus(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
reg_value = sil9034_read(priv,SLAVE0,INT_SOURCE1_ADDR) ;
sil9034_dbg("Interrupt source 1 register 0x%x = 0x%x\n",INT_SOURCE1_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,INT_SOURCE2_ADDR) ;
sil9034_dbg("Interrupt source 2 register 0x%x = 0x%x\n",INT_SOURCE2_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,INT_SOURCE3_ADDR) ;
sil9034_dbg("Interrupt source 3 register 0x%x = 0x%x\n",INT_SOURCE3_ADDR,reg_value) ;
/* Interrupt register will auto clean after read ?*/
sil9034_clearInterruptStatus(priv) ;
return 0 ;
}
int sil9034_dumpVideoConfigureStatus(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
reg_value = sil9034_read(priv,SLAVE0,HRES_L_ADDR) ;
sil9034_dbg("H resolution low register 0x%x = 0x%x\n",HRES_L_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,HRES_H_ADDR) ;
sil9034_dbg("H resolution high register 0x%x = 0x%x\n",HRES_H_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,VRES_L_ADDR) ;
sil9034_dbg("V resolution low register 0x%x = 0x%x\n",VRES_L_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,VRES_H_ADDR) ;
sil9034_dbg("V resolution high register 0x%x = 0x%x\n",VRES_H_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,DEL_L_ADDR) ;
sil9034_dbg("DE line low register 0x%x = 0x%x\n",DEL_L_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,DEL_H_ADDR) ;
sil9034_dbg("DE line high register 0x%x = 0x%x\n",DEL_H_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,POL_DETECT_ADDR) ;
sil9034_dbg("Video polarity detect register 0x%x = 0x%x\n",POL_DETECT_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,HLENGTH1_ADDR) ;
sil9034_dbg("Video HSYNC length1 register 0x%x = 0x%x\n",HLENGTH1_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,HLENGTH2_ADDR) ;
sil9034_dbg("Video HSYNC length2 register 0x%x = 0x%x\n",HLENGTH2_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,VBIT_TO_VSYNC_ADDR) ;
sil9034_dbg("Video Vbit to VSync register 0x%x = 0x%x\n",VBIT_TO_VSYNC_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,VLENGTH_ADDR) ;
sil9034_dbg("Video VSYNC length register 0x%x = 0x%x\n",VLENGTH_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,TX_TMDS_CCTRL_ADDR) ;
sil9034_dbg("TMDS C control register 0x%x = 0x%x\n",TX_TMDS_CCTRL_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,TX_TMDS_CTRL_ADDR) ;
sil9034_dbg("TMDS control register 0x%x = 0x%x\n",TX_TMDS_CTRL_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,TX_TMDS_CTRL2_ADDR) ;
sil9034_dbg("TMDS control #2 register 0x%x = 0x%x\n",TX_TMDS_CTRL2_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,TX_TMDS_CTRL3_ADDR) ;
sil9034_dbg("TMDS control #3 register 0x%x = 0x%x\n",TX_TMDS_CTRL3_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,TX_TMDS_CTRL4_ADDR) ;
sil9034_dbg("TMDS control #4 register 0x%x = 0x%x\n",TX_TMDS_CTRL4_ADDR,reg_value) ;
reg_value = sil9034_read(priv,SLAVE0,TX_VID_ACEN_ADDR) ;
sil9034_dbg("Video action enable register 0x%x = 0x%x\n",TX_VID_ACEN_ADDR,reg_value) ;
return 0 ;
}
int sil9034_dumpInterruptStateStatus(davinci6446_sil9034 *priv)
{
u8 reg_value ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
reg_value = sil9034_read(priv,SLAVE0,INT_STATE_ADDR) ;
sil9034_dbg("Interrupt state register 0x%x = 0x%x\n",INT_STATE_ADDR,reg_value) ;
if(reg_value & INT_ENABLE)
sil9034_dumpInterruptSourceStatus(priv) ;
else
sil9034_dbg("No unmask interrupt\n") ;
return 0 ;
}
int sil9034_hdcpAuthentication(davinci6446_sil9034 *priv)
{
sil9034_autoRiCheck(priv,DISABLE) ;
if(sil9034_hotplugEvent(priv))
{
sil9034_sentCPPackage(priv,ENABLE) ;
if(sil9034_checkHdcpDevice(priv) == TRUE)
{
sil9034_dbg("got 20's 1\n") ;
/* Random key */
sil9034_toggleRepeatBit(priv) ;
sil9034_releaseCPReset(priv) ;
sil9034_StopRepeatBit(priv) ;
sil9034_generateAn(priv) ;
/* Handshake start */
sil9034_readAnHdcpTx(priv) ;
sil9034_writeAnHdcpRx(priv) ;
sil9034_readAksvHdcpTx(priv) ;
sil9034_writeAksvHdcpRx(priv) ;
sil9034_readBksvHdcpRx(priv) ;
sil9034_writeBksvHdcpTx(priv) ;
if(sil9034_isRepeater(priv)==TRUE)
printk(KERN_ERR "This is repeater,not support.\n") ;
/* Finally, compare key */
mdelay(100) ; //delay for R0 calculation
if(sil9034_compareR0(priv)==FALSE)
{
priv->auth_state = REAUTH_NEED ;
}
else
{
/* unmute */
sil9034_sentCPPackage(priv,DISABLE) ;
sil9034_autoRiCheck(priv,ENABLE) ;
priv->auth_state = AUTH_DONE ;
}
}
else // no 20 ones and zeros
{
/* mute */
sil9034_sentCPPackage(priv,ENABLE) ;
sil9034_dbg("TV not send 20's 1,retry!!\n") ;
}
}
return 0 ;
}
/* HDCP key exchange for hdmi */
static void sil9034_timer(unsigned long data)
{
int status;
davinci6446_sil9034 *priv = (void *)data ;
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
if(priv)
{
#if SIL9034_SCHED
priv->work_flag = EVENT_NOTIFY ;
status = schedule_work(&priv->work);
if(!status)
printk(KERN_ERR "scheduling work error\n") ;
#else
mod_timer(&ds.timer, jiffies + TIMER_JIFFIES);
#endif
}
return ;
}
#if SIL9034_SCHED
static void sil9034_sched(void *data)
{
/* This is important, get out of the interrupt context switch trouble */
davinci6446_sil9034 *priv = container_of(data, davinci6446_sil9034, work);
u8 intr1_isr ;
u8 intr3_isr ;
switch(priv->work_flag)
{
case EVENT_NOTIFY:
intr3_isr = sil9034_read(priv,SLAVE0,INT_SOURCE3_ADDR) ;
intr1_isr = sil9034_read(priv,SLAVE0,INT_SOURCE1_ADDR) ;
/* ri frame error occur */
if(intr3_isr & (INTR3_STAT7|INTR3_STAT5|INTR3_STAT4))
{
printk(KERN_INFO "Ri frame error 0x%x\n",intr3_isr) ;
priv->auth_state = REAUTH_NEED ;
}
/* line plug */
if(intr1_isr & (INTR1_HPD|INTR1_RSEN))
{
printk(KERN_INFO "line plug 0x%x\n",intr1_isr) ;
priv->auth_state = REAUTH_NEED ;
}
break ;
default:
break ;
}
//printk(KERN_ERR "%s, %d\n",__FUNCTION__,__LINE__) ;
/* Check if hdcp authentication need */
if((priv->auth_state == AUTH_NEED) || (priv->auth_state == REAUTH_NEED))
{
sil9034_hdcpAuthentication(priv) ;
}
sil9034_dumpSystemStatus(priv) ;
//sil9034_dumpDataCtrlStatus(priv) ;
//sil9034_dumpInterruptStateStatus(priv) ;
//sil9034_dumpVideoConfigureStatus(priv) ;
/* clean the work flag */
priv->work_flag = DO_NOTHING ;
#if SIL9034_TIMER
mod_timer(&ds.timer, jiffies + TIMER_JIFFIES);
#endif
sil9034_clearInterruptStatus(priv) ;
return ;
}
#endif
void sil9034_read_table(davinci6446_sil9034 *priv, u8 slaveIndex, u8 reg, u8 tbl_cnt)
{
unsigned char i = 0;
int data;
printk("[%s]enter slaveIndex:0x%x\n", __func__, slaveIndex);
for(i = 0; i < tbl_cnt; i++){
if( (i %16 == 0)){
printk("\n");
}
data = sil9034_read(priv, slaveIndex, (reg+ i));
printk("0x%02x ", data);
}
printk("\n[%s]leave\n\n", __func__);
}
static int __init sil9034_init(void)
{
int status = 0 ;
if ((status = i2c_add_driver(&sil9034_driver)) < 0)
{
printk(KERN_INFO "%s Couldn't register SIL9034 I2C driver.\n", pname);
goto out;
}
/* Initial default as 720p */
//ds.sil9034_setting = sil9034_720p_422_embsync_setting ;
//ds.sil9034_setting = sil9034_720p_422_sepsync_setting ;
ds.sil9034_setting = sil9034_1080p_422_embsync_setting ;
/* read chip id & revision */
sil9034_chipInfo(&ds) ;
/* power down occilator */
sil9034_powerDown(&ds,ENABLE) ;
/* TMDS control register */
sil9034_hdmiTmdsConfig(&ds) ;
#if 1
/* Tune the audio input table according to DM320 hardware spec */
//sil9034_audioInputConfig() ;
/* Tune the video input table according to DM320 hardware spec */
sil9034_videoInputConfig(&ds) ;
/* software reset */
sil9034_swReset(&ds) ;
/* power up occilator */
sil9034_powerDown(&ds, DISABLE) ;
/* Trigger ROM */
sil9034_triggerRom(&ds) ;
/* software reset */
sil9034_swReset(&ds) ;
/* CEA-861 Info Frame control setting */
sil9034_cea861InfoFrameSetting(&ds) ;
/* Wake up HDMI TX */
sil9034_wakeupHdmiTx(&ds) ;
/* Sent CP package */
sil9034_sentCPPackage(&ds,ENABLE) ;
/* unmask the interrupt status */
sil9034_unmaskInterruptStatus(&ds) ;
/* Hdmi output setting */
sil9034_hdmiOutputConfig(&ds) ;
/* ddc master config */
sil9034_ddcSetting(&ds) ;
/* General control packet */
sil9034_sentCPPackage(&ds,DISABLE) ;
sil9034_cea861InfoFrameControl2(&ds,ENABLE) ;
/* HDCP control handshaking */
sil9034_hdmiHdcpConfig(&ds,ENABLE) ;
/* Disable Auto RI check here, enable it until hdcp complete. */
sil9034_autoRiCheck(&ds,DISABLE) ;
sil9034_clearInterruptStatus(&ds) ;
#endif
#if SIL9034_SCHED
INIT_WORK(&ds.work, sil9034_sched);
ds.work_flag = EVENT_NOTIFY ;
schedule_work(&ds.work);
#endif
#if SIL9034_TIMER
init_timer(&ds.timer);
ds.timer.data = (unsigned long)&ds;
ds.timer.function = sil9034_timer;
ds.timer.expires = jiffies + TIMER_JIFFIES;
add_timer(&ds.timer);
#endif
sil9034_read_table(&ds, 0, 0, 255);
out:
return status;
}
static void __exit sil9034_exit(void)
{
sil9034_dbg("----------%s----------\n",__FUNCTION__) ;
i2c_del_driver(&sil9034_driver);
if( ds.sil9034_client[0] ) kfree( ds.sil9034_client[0] );
if( ds.sil9034_client[1] ) kfree( ds.sil9034_client[1] );
}
MODULE_LICENSE("GPL");
module_init(sil9034_init);
module_exit(sil9034_exit);
Regards.