Other Parts Discussed in Thread: OMAP3530, DM3730
Hello
we are workign with OMAP3530-beagle. We compiled ti-dvsdk_omap3530-evm_4_01_00_09 for beagle board successfully. But after booting when we are running gstreamer demo under multimedia we are getting the following error and not displaying anything on the DVI..
root@beagleboard-dvsdk:~# [ 290.359130] cmemk unregistered
[ 290.535766] CMEMK module: built on Nov 6 2012 at 15:51:44
[ 290.552276] Reference Linux version 2.6.32
[ 290.563873] File /home/eswar/ti-dvsdk_omap3530-beagle_4_01_00_09/linuxutils_2_25_05_11/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c
[ 290.599121] allocated heap buffer 0xc8000000 of size 0xf00000
[ 290.618164] heap fallback enabled - will try heap if pool buffer is not available
[ 290.625732] cmemk initialized
[ 290.680938] DSPLINK Module (1.65.00.02) created on Date: Nov 6 2012 Time: 15:52:01
[ 290.791076] SDMAK module: built on Nov 6 2012 at 15:51:45
[ 290.796600] Reference Linux version 2.6.32
[ 290.805847] File /home/eswar/ti-dvsdk_omap3530-beagle_4_01_00_09/linuxutils_2_25_05_11/packages/ti/sdo/linuxutils/sdma/src/module/sdmak.c
[ 291.898956] Unable to handle kernel NULL pointer dereference at virtual address 00000000
[ 291.907104] pgd = c544c000
[ 291.909851] [00000000] *pgd=84a86031, *pte=00000000, *ppte=00000000
[ 291.916168] Internal error: Oops: 817 [#1] PREEMPT
[ 291.920989] last sysfs file: /sys/devices/platform/omapdss/manager0/display
[ 291.927978] Modules linked in: sdmak lpm_omap3530 dsplinkk cmemk ipv6 [last unloaded: sdmak]
[ 291.936523] CPU: 0 Tainted: G W (2.6.32 #1)
[ 291.941772] PC is at __down_interruptible+0x28/0xc8
[ 291.946685] LR is at down_interruptible+0x38/0x6c
[ 291.951416] pc : [<c0469f74>] lr : [<c0085f3c>] psr: 60000093
[ 291.951446] sp : c55d1ec8 ip : 00000000 fp : 0000240c
[ 291.962982] r10: c5ad4718 r9 : c55d0000 r8 : 00000000
[ 291.968231] r7 : c5ad46bc r6 : 7fffffff r5 : c49acdc0 r4 : c55d0000
[ 291.974792] r3 : 00000000 r2 : c55d0000 r1 : 00000000 r0 : c5ad4718
[ 291.981353] Flags: nZCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment user
[ 291.988616] Control: 10c5387d Table: 8544c019 DAC: 00000015
[ 291.994384] Process gst-launch-0.10 (pid: 1156, stack limit = 0xc55d02f0)
[ 292.001220] Stack: (0xc55d1ec8 to 0xc55d2000)
[ 292.005584] 1ec0: c5ad471c 00000000 c55d0000 00000000 c5ad4718 a0000013
[ 292.013824] 1ee0: 10001003 c0085f3c 00000000 bf0d51bc 10001003 bf0d4038 c541f840 00000000
[ 292.022033] 1f00: 10001003 c541f840 00000000 c55d0000 40799f50 c00efbe4 c546f400 c541f840
[ 292.030273] 1f20: 0000000c c00f02c4 c5692000 c0036f1c c006a780 00000002 80000013 00000003
[ 292.038482] 1f40: 00000000 c541f840 0000000c 00000000 00000002 c546f400 0000240c c00eeb34
[ 292.046722] 1f60: 00000000 c541f840 0000000c 00000000 10001003 c541f840 c00370c4 c55d0000
[ 292.054931] 1f80: 40799f50 c00f0340 0000000c 00000001 00000000 40799f50 00153bb4 4079c390
[ 292.063171] 1fa0: 00000036 c0036f40 40799f50 00153bb4 0000000c 10001003 00000000 00000598
[ 292.071380] 1fc0: 40799f50 00153bb4 4079c390 00000036 00002440 0013363c 40799f50 0000240c
[ 292.079620] 1fe0: ffffffff 40fabd78 4074e3c8 4050eaec 60000010 0000000c e5956010 e3560000
[ 292.087860] [<c0469f74>] (__down_interruptible+0x28/0xc8) from [<c0085f3c>] (down_interruptible+0x38/0x6c)
[ 292.097595] [<c0085f3c>] (down_interruptible+0x38/0x6c) from [<bf0d4038>] (lpm_ioctl+0x38/0x1fc [lpm_omap3530])
[ 292.107757] [<bf0d4038>] (lpm_ioctl+0x38/0x1fc [lpm_omap3530]) from [<c00efbe4>] (vfs_ioctl+0x2c/0xac)
[ 292.117095] [<c00efbe4>] (vfs_ioctl+0x2c/0xac) from [<c00f02c4>] (do_vfs_ioctl+0x570/0x5b8)
[ 292.125518] [<c00f02c4>] (do_vfs_ioctl+0x570/0x5b8) from [<c00f0340>] (sys_ioctl+0x34/0x54)
[ 292.133911] [<c00f0340>] (sys_ioctl+0x34/0x54) from [<c0036f40>] (ret_fast_syscall+0x0/0x2c)
[ 292.142425] Code: e2803004 e594500c e58d3000 e3a03000 (e581d000)
[ 292.148773] ---[ end trace 36b7f280cc874413 ]---
[ 292.153442] note: gst-launch-0.10[1156] exited with preempt_count 1
[ 292.159820] BUG: scheduling while atomic: gst-launch-0.10/1156/0x40000002
[ 292.166656] Modules linked in: sdmak lpm_omap3530 dsplinkk cmemk ipv6 [last unloaded: sdmak]
[ 292.175262] [<c003bb60>] (unwind_backtrace+0x0/0xdc) from [<c0467f08>] (schedule+0x80/0x514)
[ 292.183776] [<c0467f08>] (schedule+0x80/0x514) from [<c005c9c8>] (__cond_resched+0x14/0x20)
[ 292.192260] [<c005c9c8>] (__cond_resched+0x14/0x20) from [<c0468510>] (_cond_resched+0x30/0x40)
[ 292.201049] [<c0468510>] (_cond_resched+0x30/0x40) from [<c00cd760>] (__get_user_pages+0x1cc/0x1d8)
[ 292.210205] [<c00cd760>] (__get_user_pages+0x1cc/0x1d8) from [<c00c91b8>] (get_user_pages_fast+0x5c/0x74)
[ 292.219848] [<c00c91b8>] (get_user_pages_fast+0x5c/0x74) from [<c008f2c8>] (get_futex_key+0x98/0x150)
[ 292.229156] [<c008f2c8>] (get_futex_key+0x98/0x150) from [<c008fa10>] (futex_wake+0x44/0x130)
[ 292.238128] [<c008fa10>] (futex_wake+0x44/0x130) from [<c0091354>] (do_futex+0xc8/0xcc0)
[ 292.246307] [<c0091354>] (do_futex+0xc8/0xcc0) from [<c0092094>] (sys_futex+0x148/0x15c)
[ 292.254486] [<c0092094>] (sys_futex+0x148/0x15c) from [<c00644e4>] (mm_release+0xa4/0xb0)
[ 292.262725] [<c00644e4>] (mm_release+0xa4/0xb0) from [<c006848c>] (exit_mm+0x14/0x13c)
[ 292.270721] [<c006848c>] (exit_mm+0x14/0x13c) from [<c006a2c4>] (do_exit+0x1b4/0x69c)
[ 292.278656] [<c006a2c4>] (do_exit+0x1b4/0x69c) from [<c003a844>] (die+0x27c/0x2b0)
[ 292.286285] [<c003a844>] (die+0x27c/0x2b0) from [<c003c9a0>] (__do_kernel_fault+0x64/0x74)
[ 292.294647] [<c003c9a0>] (__do_kernel_fault+0x64/0x74) from [<c003cb74>] (do_page_fault+0x1c4/0x1d8)
[ 292.303863] [<c003cb74>] (do_page_fault+0x1c4/0x1d8) from [<c00362a8>] (do_DataAbort+0x34/0x94)
[ 292.312652] [<c00362a8>] (do_DataAbort+0x34/0x94) from [<c0036a6c>] (__dabt_svc+0x4c/0x60)
[ 292.320983] Exception stack(0xc55d1e80 to 0xc55d1ec8)
[ 292.326080] 1e80: c5ad4718 00000000 c55d0000 00000000 c55d0000 c49acdc0 7fffffff c5ad46bc
[ 292.334716] 1ea0: 00000000 c55d0000 c5ad4718 0000240c 00000000 c55d1ec8 c0085f3c c0469f74
[ 292.342956] 1ec0: 60000093 ffffffff
[ 292.346527] [<c0036a6c>] (__dabt_svc+0x4c/0x60) from [<c0469f74>] (__down_interruptible+0x28/0xc8)
[ 292.355560] [<c0469f74>] (__down_interruptible+0x28/0xc8) from [<c0085f3c>] (down_interruptible+0x38/0x6c)
[ 292.365325] [<c0085f3c>] (down_interruptible+0x38/0x6c) from [<bf0d4038>] (lpm_ioctl+0x38/0x1fc [lpm_omap3530])
[ 292.375518] [<bf0d4038>] (lpm_ioctl+0x38/0x1fc [lpm_omap3530]) from [<c00efbe4>] (vfs_ioctl+0x2c/0xac)
[ 292.384918] [<c00efbe4>] (vfs_ioctl+0x2c/0xac) from [<c00f02c4>] (do_vfs_ioctl+0x570/0x5b8)
[ 292.393341] [<c00f02c4>] (do_vfs_ioctl+0x570/0x5b8) from [<c00f0340>] (sys_ioctl+0x34/0x54)
[ 292.401763] [<c00f0340>] (sys_ioctl+0x34/0x54) from [<c0036f40>] (ret_fast_syscall+0x0/0x2c)
I searched in the internet. i didn't find any solution.
for cmemk i'm using the following command to insert using script in /etc/init.d/loadmodule-rc
modprobe cmemk phys_start=0x86300000 phys_end=0x87200000 useHeapIfPoolUnavailable=1 allowOverlap=1
There are my bootargs
setenv bootargs 'console=ttyS2,115200n8 root=/dev/mmcblk0p2 rw ip=off mem=99M@0x80000000 mmem=99M@0x88000000 purate=720 omap_vout.vid1_static_vrfb_alloc=y omapfb.mode=dvi:hd720 omapdss.def_disp=dvi omapfb.vram=0:3M rootwait'
Even when we try to run decode or encode as per OMAP3530_Software_Developers_Guide.pdf, in beagle board we are getting same error.
Please help us to solve this issue.
Thank You