Hello!
I have beaglebone board and try to launch graphic examples with NO OS from starterware. There are no graphic examples in beagelebone folder so I try to find it in another folders.
I find gaphic examples for evmAM335x in starterware (for example I try to launch 'game' example). But this examples not running at beaglebone. They say unsufficient memory.
Where I can find working graphic examples with NO OS on beaglebone?
Here is errors:
"
CortxA8: Trouble Writing Memory Block at 0x8032ee44 on Page 0 of Length 0x6534: (Error -2130 @ 0x8032EE44) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.747.0)
CortxA8: GEL: File: E:\ti\AM335X_StarterWare_02_00_00_07\binary\armv7a\cgt_ccs\am335x\evmAM335x\game\game.out: Load failed.
CortxA8: Trouble Reading Register CP15_CONTROL_REGISTER: (Error -2131 @ 0x20013F00) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.747.0)
CortxA8: Trouble Reading Memory Block at 0xc00131d6 on Page 0 of Length 0xd: (Error -1205 @ 0xC00131D4) Device memory bus has an error and may be hung. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.747.0)
CortxA8: Trouble Reading Memory Block at 0xc00131d6 on Page 0 of Length 0x8d: (Error -1044 @ 0xFFFFEC70) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.0.747.0)
CS_DAP_DebugSS: Error: (Error -5008 @ 0xFFFFEC70) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 0.0.0.0)
CortxA8: Trouble Reading Memory Block at 0xc0013152 on Page 0 of Length 0xd: (Error -1044 @ 0xFFFFEC70) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.0.747.0)
......
"