I am having problems running the client example for DSK6544. I found this example in the NDK 2.0.0 .
I would like to use it to develop a simple program that is to run on a DSK6544.
I built the client program, but upon running it in simulation it does not work as it should.
I do not have any build errors and I have done the exact steps shown in the documentation.
Could using the simulator be the problem?