Hi,
We are using OMAP4460 (1.2GHz) for one of the custom board. Our software developments are based on 4AI.1.4 OMAP4 Icecream Sandwich Release. We are facing peculiar SmartReflex problem in our boards.
If we enable the smart reflex in the kernel then few of the boards will struck while booting without any crash log. But if we disable the smart reflex in the kernel then board will boot without any crash or freeze.
In some of the boards we don't see any crash or freeze even when we enabled SmartReflex.
We found when we enable the SmartReflex, CORE and MPU voltages are going low while booting, and this is the point where OMAP stops responding and will fail to boot. We have measured the MPU and CORE voltages in two different cases and please find the below MPU and CORE voltage values measure when SmartReflex is enabled,
VDD_MPU - 0.939V
VDD_IVA - 0.853V
VDD_CORE - 0.892V
Please find the MPU and CORE voltages when SmartReflex disabled
VDD_MPU - 1.046V
VDD_IVA - 0.972V
VDD_CORE - 0.972V
We didn't find any miscellaneous voltages spikes or the drop on the voltage rails in non-working boards(When SmartReflex enabled).
SmartReflex changes CORE and MPU voltages less than 1V. Is this voltage too Low than recommended ? Are we seeing any deviation from the standard SmartReflex operation? Any suggestion to debug this issue will be appreciated.
Thanks and Regards,
Dinesh Guni