Other Parts Discussed in Thread: DM3730
I'm working with a custom board based on an Overo WaterStorm com. The processor is a DM3730. The kernel is 2.6.32 based.
I'm trying to stress test the camera ISP by rapidly opening and closing the video device with ( while true; do gst-launch v4l2src device=/dev/video0 ! video/x-raw-yuv,width=320,height=240 ! ffmpegcolorspace ! pngenc snapshot=true ! fakesink; done )
After many iterations, I will see the kernel spit out:
[ 2502.802795] Unhandled fault: external abort on non-linefetch (0x1028) at 0xfa0bce04
[ 2502.810516] Internal error: : 1028 [#1]
[ ... ]
[ 2502.846893] PC is at isp_reg_readl+0x18/0x20
[ 2502.851196] LR is at isp_reg_readl+0x10/0x20
[ ... ]
[ 2503.296447] [<c02954a0>] (isp_reg_readl+0x18/0x20) from [<c02954f8>] (isp_reg_and_or+0x1c/0x38)[ 2503.305206] [<c02954f8>] (isp_reg_and_or+0x1c/0x38) from [<c029bad0>] (isppreview_config_cfa+0x38/0x90) [ 2503.314666] [<c029bad0>] (isppreview_config_cfa+0x38/0x90) from [<c029bc5c>] (isppreview_config_datapath+0x134/0x330) [ 2503.325347] [<c029bc5c>] (isppreview_config_datapath+0x134/0x330) from [<c029be68>] (isppreview_s_pipeline+0x10/0xd0) [ 2503.336029] [<c029be68>] (isppreview_s_pipeline+0x10/0xd0) from [<c0296e98>] (isp_s_pipeline+0x1d8/0x280) [ 2503.345672] [<c0296e98>] (isp_s_pipeline+0x1d8/0x280) from [<bf036b98>] (cammux_streamon+0x218/0xa28 [cammux])
[ ... ]
The register we're trying to access here is the ISP PRV_PCR. If I try to add debug code to read ISP_CTRL right before the fault, the ISP_CTRL access faults in the same way (i.e. the whole ISP is borked, not just the previewer).
At first I thought the clocks were being disabled somehow, but tracking them seems to indicate that's not the case. Adding an early return in arch/arm/mach/omap2/clock.c omap2_dflt_clk_disable() (i.e. to disable disabling of clocks) does NOT help.
What else might I be missing? What is necessary to be able to read the ISP registers?
--Adam