This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART1 on beagleboard xm Rev c

Hi,

I want to enable uart2 on beagleboard xm rev c.

in Connector "P9"

I have setup pin mux for MCBSP3_CLKX and MCBSP3_FSX as uart2_tx and uart2_rx in beagle.c 

cat /debug/omap_mux/board/core shows the correct mux.

But it is not listing as ttyO1 all the other 3 uart s are listing as ttyO0,ttyO2,ttyO3 

Is there any thing more to do to enable uart2 .

Any help will be greatly appreciated.

Regards,

Dibin