hi,
i want to use the analog camera with OMAP4460. as OMAP4460 is having BT656, 16 bit interface, i can connect the analog camera on this port. Input which i am getting from camera modules in the form of composite video (CVBS). i saw some decoder from TI website but those converters converting CVBS signal into 10 bit BT656 only. can i connect 10 bit BT656 output from decoder to 16bit BT656? if yes what will be the implication or problem? if no then please suggest any decoder to convert this signal to 16 bit BT656.
thanks,
Ankush Agrawal