Other Parts Discussed in Thread: SYSBIOS
Hi,
I have C6747 custom legacy hardware (can't change DSPs). I'd like to use SYS/BIOS 6.x and IPC (rather than DSP/BIOS 5.x). Which SDK, PSP, etc (software) version(s) should I use? Which version of Code Composer (4 or 5)?
Searching the forums I see two strong opinions from TI employees (for different situations): 1) Use CCS 3 (not an option for me) and 2) Use CCS 5. If I use CCS 5, where do I get SYS/BIOS compatible software for C6747 (peripheral drivers, etc)? I don't see the answer on the C6747 page.
My application info, in case it is relevent: 2 x UART, 2 x SPI, 2x McASP, EMIFB SDRAM, Asynchronous EMIFA memory mapped interface, SPI Boot, GPIO, DMA, multi-threaded, IPC
Thank you,
Mike