Hello!
Which PSP I could use for SysLink and classic Beagleboard C4?
In latest SysLink RN in Validation section is that OMAP3 PSP 03.00.00.05 was used and there is also that it was tested on Beagleboard.
In http://e2e.ti.com/support/embedded/linux/f/354/t/155568.aspx is said that Beagleboard wasn't supported in this PSP version yet.
Should I use suggested in mentioned thread version PSP04.02.00.07? Or something newer?
EDIT:
And what I see additionally now in PSP 04.02.00.07... Hardware Requirement: Beagle (Rev D and later).
So what with C4?