This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Some errors about excuted APP about the codec engine?

root@dm816x-evm:/usr/share/ti/ti-codec-engine-examples/audio1_copy# ls -al

drwxrwsrwx    2 root     root         4096 Dec  9 09:42 .

drwxrwsrwx   12 root     root         4096 Dec  9 19:21 ..

lrwxrwxrwx    1 root     root           35 Jun 21  2012 all_DSP.xe674 -> ../serv

ers/all_codecs/all_DSP.xe674

-rwxrwxrwx    1 root     root      1619878 Dec  9 07:42 app_remote.xv5T

-rwxrwxrwx    1 root     root       131072 Dec  9 07:42 in.dat

root@dm816x-evm:/usr/share/ti/ti-codec-engine-examples/audio1_copy# ls

all_DSP.xe674    app_remote.xv5T  in.dat

root@dm816x-evm:/usr/share/ti/ti-codec-engine-examples/audio1_copy# ./app_remote

.xv5T

[t=0x000072db] [tid=0x40014000] xdc.runtime.Main: [+2] main> ti.sdo.ce.examples.

apps.audio1_copy

[t=0x0000747a] [tid=0x40014000] xdc.runtime.Main: [+1] App-> Application started

, procId DSP engineName remote_copy_DSP input-BUG: Your driver calls ioremap() o

n system memory.  This leads

to architecturally unpredictable behaviour on ARMv6+, and ioremap()

will fail in the next kernel release.  Please fix your driver.

file ./in.dat ou------------[ cut here ]------------

tput-file ./out.WARNING: at arch/arm/mm/ioremap.c:211 __arm_ioremap_pfn_caller+0

x58/0x190()

dat.

Modules linked in: cmemk bufferclass_ti omaplfb pvrsrvkm ipv6 ti81xxhdmi ti81xxf

b vpss syslink

Backtrace:

[<c0047b58>] (dump_backtrace+0x0/0x110) from [<c036ac0c>] (dump_stack+0x18/0x1c)

 r7:00000000 r6:c004b678 r5:c042421a r4:000000d3

[<c036abf4>] (dump_stack+0x0/0x1c) from [<c006a7b0>] (warn_slowpath_common+0x54/

0x6c)

[<c006a75c>] (warn_slowpath_common+0x0/0x6c) from [<c006a7ec>] (warn_slowpath_nu

ll+0x24/0x2c)

 r9:00000002 r8:00000000 r7:bf035b6c r6:0008b000 r5:0008df40

r4:00000000

[<c006a7c8>] (warn_slowpath_null+0x0/0x2c) from [<c004b678>] (__arm_ioremap_pfn_

caller+0x58/0x190)

[<c004b620>] (__arm_ioremap_pfn_caller+0x0/0x190) from [<c004b834>] (__arm_iorem

ap_caller+0x64/0x6c)

[<c004b7d0>] (__arm_ioremap_caller+0x0/0x6c) from [<c005d6c8>] (omap_ioremap+0x6

0/0x64)

 r6:00000000 r5:0008df40 r4:8b000000

[<c005d668>] (omap_ioremap+0x0/0x64) from [<bf035b6c>] (MemoryOS_map+0x1e0/0x398

 [syslink])

 r7:cb63bcd8 r6:00000000 r5:cb63bc70 r4:d0889000

[<bf03598c>] (MemoryOS_map+0x0/0x398 [syslink]) from [<bf0044d4>] (_ProcMgr_map+

0x1cc/0x4a0 [syslink])

 r8:00000003 r7:cb63bcd8 r6:00000000 r5:06a85000 r4:cb63bd54

[<bf004308>] (_ProcMgr_map+0x0/0x4a0 [syslink]) from [<bf012874>] (ElfLoaderTrgW

rite_copy+0x13c/0x3a0 [syslink])

[<bf012738>] (ElfLoaderTrgWrite_copy+0x0/0x3a0 [syslink]) from [<bf015bf8>] (DLI

F_copy+0x18/0x24 [syslink])

[<bf015be0>] (DLIF_copy+0x0/0x24 [syslink]) from [<bf014914>] (DLOAD_load+0x834/

0xaa8 [syslink])

[<bf0140e0>] (DLOAD_load+0x0/0xaa8 [syslink]) from [<bf011ac4>] (ElfLoader_load+

0x270/0x330 [syslink])

[<bf011854>] (ElfLoader_load+0x0/0x330 [syslink]) from [<bf0022d0>] (Loader_load

+0xec/0x164 [syslink])

[<bf0021e4>] (Loader_load+0x0/0x164 [syslink]) from [<bf0068f4>] (ProcMgr_load+0

x21c/0x2f8 [syslink])

[<bf0066d8>] (ProcMgr_load+0x0/0x2f8 [syslink]) from [<bf0089b0>] (ProcMgrDrv_io

ctl+0xc8c/0x1cc8 [syslink])

[<bf007d24>] (ProcMgrDrv_ioctl+0x0/0x1cc8 [syslink]) from [<c00cfb40>] (vfs_ioct

l+0x28/0x44)

 r8:400dbcb8 r7:00000008 r6:00000008 r5:cb48b900 r4:00000000

[<c00cfb18>] (vfs_ioctl+0x0/0x44) from [<c00d0250>] (do_vfs_ioctl+0x500/0x540)

[<c00cfd50>] (do_vfs_ioctl+0x0/0x540) from [<c00d02e8>] (sys_ioctl+0x58/0x7c)

[<c00d0290>] (sys_ioctl+0x0/0x7c) from [<c0043da0>] (ret_fast_syscall+0x0/0x30)

 r8:c0043f48 r7:00000036 r6:0000f938 r5:00000001 r4:00000000

---[ end trace ffd00d3afb53ee22 ]---