This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

If I can connect these two AM3359 through EMIF ? there are large amounts of data must transmit from one AM3359 to another AM3359 soc.

Other Parts Discussed in Thread: AM3359

We design an industry  PLC ,the board use two  AM3359  soc,there are  large amounts of data must  transmit from one AM3359 to another AM3359 soc.But I don't want to use the USB or Ethernet ... to transmit the amounts of data , I think if I can use the EMIF to connect  these two AM3359  each other,I want to transmit the large amount data each other through the EMIF ?When the machine running,I want set one AM3359 as the mast ,the NO2 AM3359 set as slave,then exchange the data through the EMIF  . If I can connect these two AM3359 through EMIF ? If it is impossible , is there a good method to connect this two AM3359 ?