This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OAL Cache Test failure for WEC7 AM335x EVM BSP

Hi,

I am executing some predefined test cases using windows embedded compact test kit, but some of the test's are getting failed 

e.g

OAL No Cache Test - 1103,1104,1105 - failed

Is there any issue with these tests ? OAL cache implementation for this BSP ? 

Actually I am getting some prefetch abort exceptions , stack overflow exceptions, for IE as well as with other simple applications. even I have tried simplest application which just allocate some memory , initialize it and frees it. 

and so thought may be will get some pointers after going through CTK tests.

Thanks