Hello,
Is is possible to merge u-boot, kernel, filesystem into one merged binary which will be programeed in target ?
Thanks,
Ran
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Typically I only see this on components such as NAND, NOR etc prior to them being placed on the board. Is this a manufacturing question in terms of how to images onto the target during manufacturing?
It might be. If there any other peripherals that could be used for booting such as an SD card.
If you have an SD card and can boot from it you might be able to use the "dd" command to save off the entire image to SD card, and then place the SD card in the next board board and use the "dd" command to write the image.
What are the peripherals you have available?