This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VHDL (FPGA) module/addons for Pandaboard ES !



Dear Sir,

I am using Panadaboard ES. I have ported  my own compiled LFS (linux from scratch) and it is working well as per my requirement. I found out that there are GPIO available in pandaboard, but the problem is it is available in different Address Block. i.e. Not a continuous GPIO in single address. If it will be a contineous on single Address, I can operate the whole GPIO bank from user space or may be kernel module, but is is not possible in Pandaboard to operate GPIO Bank.

It will be great If there is any extension/ad-dons/module available for GPIO , so that I can attach to the board and drive my hardware OR is there any VHDL/FPGA extension/ad-dons/module available for Pandaboard?

I need to operate my Hardware which require 40 pin, So It will be great If I can operate GPIO in Bank or via VHDL to minimize the delay in operating the Hardware.

Kindly please Guide me in right direction.

Look forward to hear from you soon.

Thanks & Regards,

Suresh