This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issue running HUA on TMDXEVM6657L

Other Parts Discussed in Thread: TEST2

Hi all,

I found some issue about HUA on TMDXEVM6657L.

MCSDK                         2.1.1.4

PDK C6657                  1.1.1.4

NDK                                2.21.1.38

SYS/BIOS                       6.33.6.50

(1)User Switch 1 no effect

Test1:         Didn`t use CCS.     User Switch 1 "on"--------it runs in DHCP mode         Using putty connect it

                     I can connect WEB. But Throughput test still Waiting for receiver to get ready.....

Test2:         Didn`t use CCS.     User Switch 1 "off"--------it runs in Static IP mode      Using putty connect it

                    Still in DHCP mode.Throughput test still Waiting for receiver to get ready.....

Test3:         Use CCS.     User Switch 1 "off"--------it runs in Static IP mode     Check CIO

                    Still in DHCP mode.Throughput test still Waiting for receiver to get ready.....

So I change the code in HUA project (!platform_get_switch_state(1)) for using Static IP mode.

(2)Throughput Test still Waiting for receiver to get ready.....

I config DSP in UDP/TCP TX mode and loopback,and in same subnet,Gateway.

I use Wireshark to capture.But noting captured except config DSP data when using WEB.

I set it in loopback mode. And I use tools send data from PC to DSP. I can get the loopback data from DSP.

I`m so confuse. I want to test throughput. And it have waste my many time.

Please Help me...

Best Regards,

Li