This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Why I always meet frame sync error that I learn for McASP control with beaglebone?

I use beaglebone to learn for McASP control, with transmit burst mode.

Then base on my program, I can measure correct serial stream data "0x5A085A66" from AXR0, and correct frame signal from FSX.

But I always meet frame sync error due to XSTAT-bit1=1 after Release the Transmit State machine and frame sync generator from reset.

Please check the following my code, how I can correct it.

int main(void) {  

MCASP0ModuleClkConfig();  

MCASP0PinMuxSetup();  

McASPTxReset(SOC_MCASP_0_CTRL_REGS);

   McASPTxFmtMaskSet(SOC_MCASP_0_CTRL_REGS, (1 << 32) - 1);

   McASPTxFmtSet(SOC_MCASP_0_CTRL_REGS, (MCASP_TX_PAD_WITH_0 | MCASP_TX_BITSTREAM_MSB_FIRST                              | MCASP_TX_SYNC_DELAY_1BIT | (32 >> 2)                              | ((32/2 -1) << MCASP_XFMT_XSSZ_SHIFT)                              | MCASP_TX_BUF_PERICONFIGPORT));

    /* Configure the frame sync. Burst mode = 0 */    

McASPTxFrameSyncCfg(SOC_MCASP_0_CTRL_REGS, 0, MCASP_TX_FS_WIDTH_WORD,       MCASP_TX_FS_INT_BEGIN_ON_RIS_EDGE);

    McASPTxClkCfg(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLK_INTERNAL, 0, 0);    

 McASPTxClkPolaritySet(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLK_POL_RIS_EDGE);    

McASPTxClkCheckConfig(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLKCHCK_DIV32, 0x00, 0xFF);      

/* Disable synchronization of RX and TX sections  */    

McASPTxRxClkSyncDisable(SOC_MCASP_0_CTRL_REGS);

    /* Enable the transmitter/receiver slots */    

McASPTxTimeSlotSet(SOC_MCASP_0_CTRL_REGS, 1);

    McASPSerializerTxSet(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_TX);

    McASPPinMcASPSet(SOC_MCASP_0_CTRL_REGS, 0xFFFFFFFF);    

McASPPinDirOutputSet(SOC_MCASP_0_CTRL_REGS, MCASP_PIN_AXR(MCASP_XSER_TX));    

McASPPinDirOutputSet(SOC_MCASP_0_CTRL_REGS, MCASP_PIN_ACLKX                                          | MCASP_PIN_AFSX);

    McASPPinDirInputSet(SOC_MCASP_0_CTRL_REGS,                                                 MCASP_PIN_AFSR                                                | MCASP_PIN_ACLKR                                                | MCASP_PIN_AXR(MCASP_XSER_RX));

    McASPTxClkStart(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLK_INTERNAL);

    // Activate the  serializers    

   McASPTxSerActivate(SOC_MCASP_0_CTRL_REGS);

   McASPTxBufWrite(SOC_MCASP_0_CTRL_REGS, 0, 0x5A085A66);

    while(McASPTxStatusGet(SOC_MCASP_0_CTRL_REGS) & MCASP_TX_STAT_DATAREADY);

    // Activate the state machines    

McASPTxEnable(SOC_MCASP_0_CTRL_REGS);        

while(1);

} 

Best Regards,
Alan