Other Parts Discussed in Thread: DM3730
We are bringing up a 2nd generation board and are having trouble booting.
We are able to erase flash and program the boot loader into flash using the device USB port.
When we try to boot the start up sequence works normally and we do come out of reset. Then we go back into reset about every 2.2ms.
During the boot up we get a couple of chip selects to the flash and then we go back into reset. The chip slect and cle siginals are clean, the data is clean while the cle is transitioning. When the cle goes high and stops activiety the data lines rise to high very slowly. But I think this is just the bus being released when there is no activity. We did not change the flash part number between revisions. We did change DRAM but I believe this failure is happening well before the dram is accessed.
Any feedback on how to trouble shoot this would be helpful. This all happens before the os or application software is running.
Thanks