This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

A problem in the ethernet port



Hi all,

I am using a custom board based on dm368. capture and encode are in 1080P @ 26 fps, that is OK for me.

The h264 encode bitrate is set to 8M.

But I can't send out the video at the same speed, only about 20 fps can be sent out.

There seems a problem in the ethernet port. I take a test getting a result that it can send out data
at bitrate of 14M. the test is done with no capture.

I guess that the ethernet port's sending speed gets slow down when capturing video.

what's problem ? any clue ?