Other Parts Discussed in Thread: TMS320F28335
Hi,
I am looking for an example build with multitask based on bios.
I hope that example can run well on control28335 plform.
thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320F28335
Hi,
I am looking for an example build with multitask based on bios.
I hope that example can run well on control28335 plform.
thank you.
what's the version of your ccs, my ccs is 4.1.2 and I can't find this task example.
can you send me this task example.
thank you.
Hi Yefu,
If I export the project, it will still depend on which version of SYS/BIOS you have. The wizard may look a bit different in CCS 4.1, but if you have a version of SYS/BIOS (and XDCtools) that supports 28335 then it should be available.
Which version of SYS/BIOS and XDCtools are you using?
Hi Yefu,
Yefu said:DSP/BIOS is 5.41.20.14
I'm not familiar with DSP/BIOS 5.41.20..
DSP/BIOS 5.41.11.39 or greater has support for the F28355. When you create a new project for your part, you should see DPS/BIOS v5.xx Examples. If you're having problems finding the examples, it may be possible that CCS wasn't able to find the DSP/BIOS installation. In which directory was it installed in?