Other Parts Discussed in Thread: TPS65910A, AM3359, TPS65910
Hi,
We are using an AM3359 and a TPS65910A. We have a 32kHz clock on the TPS65910A and no clock on the AM3359 (we have RTC_XTALIN pulled low and RTX_XTALOUT disconnected per the datasheet). We are, however, feeding VRTC from the TPS65910A to the VDDS_RTC on the AM3359 in order to make use of the PMIC_POWER_EN output to enable the TPS65910A.
We are observing a very high current draw (~350 uA) on the VDD_RTC path between the TPS65910 and the AM3359. We really can't figure out where the leakage is coming from. This is a serious problem as we would like to power the TPS65910A VBACKUP with a coin cell in order to maintain time and the current consumption is entirely too high.
Looking at the current measurements on the AM3359 wiki, http://processors.wiki.ti.com/index.php/AM335x_Power_Consumption_Summary, the VDDS_RTC current measured on the EVM is fairly consistent (>300 uA) with what we are seeing. This is not surprising as we based most of our TPS65910A/AM3359 interconnect based on the EVM. Is this really what we should expect for an RTC power domain, or is there an issue with the EVM schematic?
We have tested this using TMX parts as well as Rev 1.0 Silicon.
-Mike